2368754_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2368754_en-US

2368754_en-US

[S32DS 3.6.7] S32K1xx RTD 3.0.0 not detected when creating new project

Hello everyone,

I am having issues with S32 Design Studio 3.6.7 and the S32K1xx RTD Drivers version 3.0.0.

Current setup:

  • S32 Design Studio version: 3.6.7

  • Device: S32K1xx family

  • RTD Drivers version: 3.0.0

  • OS: Windows 11

The RTD does not appear in the SDK selection when creating a new project.

Has anyone experienced the same issue or found a solution?

Thank you very much for your support.

antonio_esal_0-1779307200727.png

antonio_esal_1-1779307210251.png



Antonio

Re: [S32DS 3.6.7] S32K1xx RTD 3.0.0 not detected when creating new project

Hi Julián,

You were correct — the issue was that S32DS comes with GCC 11. I installed GCC 10.2, and everything is working properly now.

Thank you for your help.

antonio_esal_0-1779317981160.png

antonio_esal_1-1779317996701.png


Re: [S32DS 3.6.7] S32K1xx RTD 3.0.0 not detected when creating new project

Hi @antonio_esal,

When installing the RTD packages, have you made sure the correct NXP GCC version has been installed? Out of the box, S32DS 3.6.0 and up comes with NXP GCC 11.4, however, S32K1 RTD 3.0.0 has been built and tested with NXP GCC 10.2 (As noted in the release notes):

Julin_AragnM_4-1779314320497.png

Julin_AragnM_0-1779314190029.png

When creating a new S32DS application, make sure the correct toolchain is selected:

Julin_AragnM_1-1779314212399.png

Julin_AragnM_2-1779314218822.png

If this is not the root cause of your issue, please share your installation details (Help > Installation Details) so I can confirm all of the required dependencies for S32K1 RTD are installed.

Best regards,
Julián

Tags (1)
No ratings
Version history
Last update:
‎05-21-2026 04:33 AM
Updated by: