Hello,
I am currently working on a GUI for a wearable using lvgl, zephyr and GUI-Guider.
We would like to have some more complex animations in our project, which are hard to recreate from scratch with the existing widgets and for that purpose we would like to implement small videos we can just drop into the UI when needed.
I already was able to create a POC by converting a video to a series of pictures, but that takes a lot of flash space, as the compression is very limited that way.
The idea was to use a better format like h264 or similar. But the support for that seems to be limited to the i.MX RT1050 out of the box.
Is there some way to also get this running on the mimxrt595s, or does it not make sense? My research led me to believe, that it is not possible without linking ffmpeg libraries to our lvgl implementation, which surely would take some porting effort and take too much flash and RAM from our chip to make any sense.
Am I right in this last assumption or is there a way to save resources in our situation?
Best regards,
Kai