2368090_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2368090_en-US

2368090_en-US

Can FRDM-MCXN947 connect to LCD-PAR-S035 via J7 PMOD

Can FRDM-MCXN947 connect to LCD-PAR-S035 via J7 PMOD? Is there any relevant Zephyr example? #LVGL

MCXNRe: Can FRDM-MCXN947 connect to LCD-PAR-S035 via J7 PMOD

You are welcome. Any new issues, welcome to create a new post.

Re: Can FRDM-MCXN947 connect to LCD-PAR-S035 via J7 PMOD

Thanks for your reply. FRDM-MCXN947 connect to LCD-PAR-S035 via J8 connector works well.

Re: Can FRDM-MCXN947 connect to LCD-PAR-S035 via J7 PMOD

Hello @chaohang021 ,

Thanks for your post. 

No, on FRDM-MCXN947, the LCD-PAR-S035 is not the J7 Pmod connection path. The board user manual says the LCD display support is on the 28-pin FlexIO header J8 , and explicitly states that this header is intended to support the LCD-PAR-S035 display. The J7 header is documented separately as a general Pmod header for connecting peripheral modules , not as the LCD_PAR_S035 connection for this board.

Celeste_Liu_0-1779273159024.png

Yes, the NXP Zephyr display portability demo and the Zephyr LVGL demo flow for FRDM-MCXN947 + LCD-PAR-S035 are relevant. For FRDM-MCXN947, the Zephyr/LVGL example uses samples/modules/lvgl/demos with Board: FRDM MCXN947 (CPU0) and SHIELD="lcd_par_s035_8080".

Hope it helps.

BR

Celeste


タグ(1)
評価なし
バージョン履歴
最終更新日:
木曜日
更新者: