Running both Android + Linux as DomU's on i.MX95 EVK or i.MX8QMI am checking the applicability of running both Android Automotive and Linux guest OSes on top of Xen hypervisor.
- There are some conflicting information on between release notes, and user guides, In the release note of the Android Automotive, there is an "N" on both i.MX8QM and i.MX95 for Virtualization Android, while it is clearly instructed in the user guide how to run Android over Xen:

I want to answer the question whether it is supported or not, but I cannot accurately decide based on different documents, older documents says its supported even for i.MX8QM and newer ones says no. - It is mentioned in the user guide that you can run Linux Guest or Android Automotive Guest, but its not mentioned whether they can coexist at the same time (2 DomUs). Please tell me if this is possible in i.MX95 or i.MX8QM or both.
- As mentioned in question 1, for the i.MX 8QuadMax, it was mentioned in old documents that it can run Android VM over Xen, but that was for Android 9 or Android 10. In recent documentation it is stated as "N" in the Android VM over Xen and the user guide shows instuctions only for i.mx 95, is there a reason that it cannot run newer Android versions?
Androidi.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusLinuxRe: Running both Android + Linux as DomU's on i.MX95 EVK or i.MX8QMHello,
1> it is correct in older releases of Android we had i.MX8 XEN support as a demo/reference, but we no longer support it in new Android releases. While in the other case for the i.MX95 we do have support in the new releases.
2> As said above, for old releases it may be possible for the i.MX8, as for the i.MX95 is not officially supported, but technically feasible with custom integration.
3> It is related to 1) officially XEN for the i.MX8 was releases as a demo/reference, with changes to new android releases the focus was switched to the new i.MX95.
Best regards/Saludos,
Aldo.
Re: Running both Android + Linux as DomU's on i.MX95 EVK or i.MX8QMHello, thank you for the quick response!
So for i.MX95, only Dom0 (linux, which is not thin as I can see from the documents) + DomU (Android) is officially supported. Is it possible to attach a display to the Dom0 and another one to DomU?
Do you have any plans to support 2 DomU's in the future for i.MX95?