2366808_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2366808_en-US

2366808_en-US

Problem in changing fps from 30 to 60 fps for mx95mbcam with imx95

I am using imx95 with mx95mbcam camera module with gmsl maixm serdes.
The default working driver is running with 1920*1280@30 fps, I wanted to run it with  1920*1280@60 fps. I made the changes in the 0x03c10 sensor register, but the maximum I was able to achieve was 47fps. After that, I was not able to get a video feed.
Is there any limitation with Maxim SerDes or any other problem?

Re: Problem in changing fps from 30 to 60 fps for mx95mbcam with imx95

This may be a bandwidth issue. How many cameras you connect to the Maxim DES? By default, it should run at 1.5Gbps * 4lanes.

Re: Problem in changing fps from 30 to 60 fps for mx95mbcam with imx95

connected 4 cameras, but running only 1 cam.
1920*1280 resolution. raw 16-bit PWL output from sensor.

Tags (1)
No ratings
Version history
Last update:
Thursday
Updated by: