2366644_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2366644_en-US

2366644_en-US

RT1189 with TSN

Hi there, I am trying to build a project with RT1189/RT1186.The goal is to receive data from a netc port and send it through another netc port with tsn. Is there any tsn examples inside sdk to refer to? Thank you.

Board DesignDevelopment BoardRe: RT1189 with TSNHi Gavin,

Thank you so much for replying. I will definitely go looking to those examples you suggest.

Best regards.
Re: RT1189 with TSN

Hi @alex_l1 ,

Thanks for your interest in NXP MIMXRT sereis! 

For RT1189, there are NETC examples available in the MCUXpresso SDK.

If your requirement is to receive frames from one NETC port and forward them to another NETC port, the closest SDK example is:

  driver_examples/netc/switch
 
This example demonstrates how to configure NETC as a network switch.

 

You may also refer to:
  driver_examples/netc/txrx_transfer
  driver_examples/netc/psi_vsi_message

 

Please note that these examples are NETC driver-level examples. They are useful for NETC port TX/RX and switch forwarding, but they are not a full TSN protocol stack demo.

 

If you need actual TSN protocol features, such as gPTP, AVB/TSN endpoint, TSN bridge, stream reservation, or scheduled traffic, please refer to the NXP GenAVB/TSN middleware with detailed guides in RT1180 page:

 

https://www.nxp.com/products/i.MX-RT1180

Gavin_Jia_0-1779158556163.png

 

Hope that helps!
 
Best regards,
Gavin

 

Best regards,

タグ(1)
評価なし
バージョン履歴
最終更新日:
1週間前
更新者: