when I plugin 1 camera I can bring up the camera, but I plugin 2 cameras (same module), all the cameras bring up failed.
log info:
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[0:00:31.239670305] [973] INFO Camera camera.cpp:1215 configuring streams: (0) 1920x1536-YUYV/Unset
[0:00:31.250185346] [972] ERROR V4L2 v4l2_videodevice.cpp:1991 /dev/video0[15:cap]: Failed to start streaming: Broken pipe
ERROR: from element /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: Failed to start the camera: Broken pipe
Additional debug info:
../src/gstreamer/gstlibcamerasrc.cpp(871): gst_libcamera_src_task_enter (): /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0:
Camera.start() failed with error code -32
Execution ended after 0:00:00.012442958
Setting pipeline to NULL ...
Freeing pipeline ...
When two max9295a cameras are connected to same MAX96724, only Frame Sync mode can work, free run will not work in multiple camera use case on MAX96724.
In fact, the main loading to debug the MAX96724 is on the setting between camera (MAX9295a) and MAX96724, I think customer maybe need support from Maxim. Before Linux can work, they should make sure MAX96724's LOCK bit is set without error, only after that, MAX96724 can output MIPI video frames to iMX95.
What's the camera sensor? Are they set to Frame Sync mode in driver? Some camera are working in free run in default, in this case, single camera can work on MAX96724 directly, but for multiple cameras, MAX96724 needs they work in Frame Sync mode, all the cameras should send out video frame after they received the SYNC signal from MAX96724.
And what's the media-ctl command the customer used?
Yes, the GMSL2 Link A&B is Locked for max96724 -> 2 max9295a cameras.
driver log:
[ 9.882277] max96724 3-0027: GMSL link mask: configured = 0xf, locked = 0x3
driver code:
the camera with max9295a,is working in free run, no frame sync need.
cam -l , media-ctl & gst log info:
root@imx95evk:~# cam -l
[0:01:54.016285137] [1058] WARN IPAManager ipa_manager.cpp:148 No IPA found in '/media/jeffin/dev-work/nxp/codeaurora/libcamera/install/lib/libcamera/ipa'
[0:01:54.016504762] [1058] INFO Camera camera_manager.cpp:330 libcamera v0.0.0+6194-lf-6.12.49-2.2.0-dirty (2026-04-24T21:03:02CST)
[0:01:54.061756845] [1059] WARN CameraSensor camera_sensor_legacy.cpp:502 'mx95wecam 8-0062': No sensor delays found in static properties. Assuming unverified defaults.
[0:01:54.061982970] [1059] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x00980911 but control is not exposed by device /dev/v4l-subdev12
[0:01:54.062069678] [1059] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x009e0903 but control is not exposed by device /dev/v4l-subdev12
[0:01:54.068941887] [1059] WARN CameraSensor camera_sensor_legacy.cpp:502 'mx95wecam 9-0062': No sensor delays found in static properties. Assuming unverified defaults.
[0:01:54.069094470] [1059] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x00980911 but control is not exposed by device /dev/v4l-subdev13
[0:01:54.069152970] [1059] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x009e0903 but control is not exposed by device /dev/v4l-subdev13
[0:01:54.073940928] [1059] INFO Camera camera_manager.cpp:220 Adding camera '/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@0/mx95wecam@62' for pipeline handler simple
[0:01:54.074970262] [1059] INFO Camera camera_manager.cpp:220 Adding camera '/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@1/mx95wecam@62' for pipeline handler simple
Available cameras:
1: 'mx95wecam' (/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@0/mx95wecam@62)
2: 'mx95wecam' (/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@1/mx95wecam@62)
root@imx95evk:~# media-ctl -d /dev/media0 -p
Media controller API version 6.12.49
Media device information
------------------------
driver mxc-isi
model FSL Capture Media Device
serial
bus info platform:4ad50000.isi
hw revision 0x0
driver version 6.12.49
Device topology
- entity 1: crossbar (13 pads, 10 links, 8 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev0
routes:
2/0 -> 5/0 [ACTIVE]
2/0 -> 6/0 [ACTIVE]
2/0 -> 7/0 [ACTIVE]
2/0 -> 8/0 [ACTIVE]
2/0 -> 9/0 [ACTIVE]
2/0 -> 10/0 [ACTIVE]
2/0 -> 11/0 [ACTIVE]
2/0 -> 12/0 [ACTIVE]
pad0: SINK,MUST_CONNECT
pad1: SINK,MUST_CONNECT
pad2: SINK,MUST_CONNECT
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
<- "4ac10000.syscon:formatter@20":1 [ENABLED,IMMUTABLE]
pad3: SINK,MUST_CONNECT
pad4: SINK,MUST_CONNECT
<- "mxc_isi.output":0 [ENABLED,IMMUTABLE]
pad5: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.0":0 [ENABLED,IMMUTABLE]
pad6: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.1":0 [ENABLED,IMMUTABLE]
pad7: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.2":0 [ENABLED,IMMUTABLE]
pad8: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.3":0 [ENABLED,IMMUTABLE]
pad9: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.4":0 [ENABLED,IMMUTABLE]
pad10: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.5":0 [ENABLED,IMMUTABLE]
pad11: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.6":0 [ENABLED,IMMUTABLE]
pad12: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:srgb xfer:srgb ycbcr:601 quantization:lim-range]
-> "mxc_isi.7":0 [ENABLED,IMMUTABLE]
- entity 15: mxc_isi.0 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev1
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":5 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.0.capture":0 [ENABLED,IMMUTABLE]
- entity 18: mxc_isi.0.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video0
pad0: SINK
<- "mxc_isi.0":1 [ENABLED,IMMUTABLE]
- entity 26: mxc_isi.1 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev2
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":6 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.1.capture":0 [ENABLED,IMMUTABLE]
- entity 29: mxc_isi.1.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video1
pad0: SINK
<- "mxc_isi.1":1 [ENABLED,IMMUTABLE]
- entity 37: mxc_isi.2 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev3
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":7 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.2.capture":0 [ENABLED,IMMUTABLE]
- entity 40: mxc_isi.2.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video2
pad0: SINK
<- "mxc_isi.2":1 [ENABLED,IMMUTABLE]
- entity 48: mxc_isi.3 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev4
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":8 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.3.capture":0 [ENABLED,IMMUTABLE]
- entity 51: mxc_isi.3.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video3
pad0: SINK
<- "mxc_isi.3":1 [ENABLED,IMMUTABLE]
- entity 59: mxc_isi.4 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev5
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":9 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.4.capture":0 [ENABLED,IMMUTABLE]
- entity 62: mxc_isi.4.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video4
pad0: SINK
<- "mxc_isi.4":1 [ENABLED,IMMUTABLE]
- entity 70: mxc_isi.5 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev6
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":10 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.5.capture":0 [ENABLED,IMMUTABLE]
- entity 73: mxc_isi.5.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video5
pad0: SINK
<- "mxc_isi.5":1 [ENABLED,IMMUTABLE]
- entity 81: mxc_isi.6 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev7
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":11 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.6.capture":0 [ENABLED,IMMUTABLE]
- entity 84: mxc_isi.6.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video6
pad0: SINK
<- "mxc_isi.6":1 [ENABLED,IMMUTABLE]
- entity 92: mxc_isi.7 (2 pads, 2 links, 0 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev8
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
compose.bounds:(0,0)/1920x1536
compose:(0,0)/1920x1536]
<- "crossbar":12 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:YUV8_1X24/1920x1536 field:none colorspace:jpeg xfer:srgb ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "mxc_isi.7.capture":0 [ENABLED,IMMUTABLE]
- entity 95: mxc_isi.7.capture (1 pad, 1 link)
type Node subtype V4L flags 0
device node name /dev/video7
pad0: SINK
<- "mxc_isi.7":1 [ENABLED,IMMUTABLE]
- entity 103: mxc_isi.output (1 pad, 1 link)
type Node subtype V4L flags 0
pad0: SOURCE
-> "crossbar":4 [ENABLED,IMMUTABLE]
- entity 110: 4ac10000.syscon:formatter@20 (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev9
routes:
0/0 -> 1/0 [ACTIVE]
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
<- "csidev-4ad30000.csi":1 [ENABLED,IMMUTABLE]
pad1: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
-> "crossbar":2 [ENABLED,IMMUTABLE]
- entity 115: csidev-4ad30000.csi (2 pads, 2 links, 1 route)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev10
routes:
0/0 -> 1/0 [ACTIVE]
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
<- "max96724 3-0027":4 [ENABLED]
pad1: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1080 field:none colorspace:smpte170m xfer:709 ycbcr:601 quantization:lim-range]
-> "4ac10000.syscon:formatter@20":0 [ENABLED,IMMUTABLE]
- entity 120: max96724 3-0027 (6 pads, 3 links, 4 routes)
type V4L2 subdev subtype Unknown flags 0
device node name /dev/v4l-subdev11
routes:
0/0 -> 4/0 [ACTIVE]
1/0 -> 4/1 [ACTIVE]
2/0 -> 5/2 [ACTIVE]
3/0 -> 5/3 [ACTIVE]
pad0: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
<- "mx95wecam 8-0062":0 [ENABLED,IMMUTABLE]
pad1: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
<- "mx95wecam 9-0062":0 [ENABLED,IMMUTABLE]
pad2: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
pad3: SINK
[stream:0 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
pad4: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
[stream:1 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
-> "csidev-4ad30000.csi":0 [ENABLED]
pad5: SOURCE
[stream:2 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
[stream:3 fmt:UYVY8_1X16/1920x1536 colorspace:raw]
- entity 129: mx95wecam 8-0062 (1 pad, 1 link, 0 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev12
pad0: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:raw xfer:none ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "max96724 3-0027":0 [ENABLED,IMMUTABLE]
- entity 133: mx95wecam 9-0062 (1 pad, 1 link, 0 routes)
type V4L2 subdev subtype Sensor flags 0
device node name /dev/v4l-subdev13
pad0: SOURCE
[stream:0 fmt:UYVY8_1X16/1920x1536 field:none colorspace:raw xfer:none ycbcr:601 quantization:full-range
crop.bounds:(0,0)/1920x1536
crop:(0,0)/1920x1536]
-> "max96724 3-0027":1 [ENABLED,IMMUTABLE]
root@imx95evk:~# gst-launch-1.0 libcamerasrc camera-name=/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@0/mx95wecam@62 ! video/x-raw,width=1920,height=1536,format=YUY2 ! autovid
eosink
Setting pipeline to PAUSED ...
[0:03:53.646204235] [1061] WARN IPAManager ipa_manager.cpp:148 No IPA found in '/media/jeffin/dev-work/nxp/codeaurora/libcamera/install/lib/libcamera/ipa'
[0:03:53.646456819] [1061] INFO Camera camera_manager.cpp:330 libcamera v0.0.0+6194-lf-6.12.49-2.2.0-dirty (2026-04-24T21:03:02CST)
[0:03:53.694436152] [1068] WARN CameraSensor camera_sensor_legacy.cpp:502 'mx95wecam 8-0062': No sensor delays found in static properties. Assuming unverified defaults.
[0:03:53.694678277] [1068] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x00980911 but control is not exposed by device /dev/v4l-subdev12
[0:03:53.694785485] [1068] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x009e0903 but control is not exposed by device /dev/v4l-subdev12
[0:03:53.702510985] [1068] WARN CameraSensor camera_sensor_legacy.cpp:502 'mx95wecam 9-0062': No sensor delays found in static properties. Assuming unverified defaults.
[0:03:53.702685235] [1068] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x00980911 but control is not exposed by device /dev/v4l-subdev13
[0:03:53.702777610] [1068] ERROR DelayedControls delayed_controls.cpp:87 Delay request for control id 0x009e0903 but control is not exposed by device /dev/v4l-subdev13
[0:03:53.708162819] [1068] INFO Camera camera_manager.cpp:220 Adding camera '/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@0/mx95wecam@62' for pipeline handler simple
[0:03:53.709431777] [1068] INFO Camera camera_manager.cpp:220 Adding camera '/base/soc/bus@42000000/i2c@42540000/max96724@27/i2c-mux/i2c@1/mx95wecam@62' for pipeline handler simple
Pipeline is live and does not need PREROLL ...
Pipeline is PREROLLED ...
Setting pipeline to PLAYING ...
New clock: GstSystemClock
[0:03:53.713476694] [1069] INFO Camera camera.cpp:1215 configuring streams: (0) 1920x1536-YUYV/Unset
[0:03:53.724398360] [1068] ERROR V4L2 v4l2_videodevice.cpp:1991 /dev/video0[15:cap]: Failed to start streaming: Broken pipe
ERROR: from element /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0: Failed to start the camera: Broken pipe
Additional debug info:
../src/gstreamer/gstlibcamerasrc.cpp(871): gst_libcamera_src_task_enter (): /GstPipeline:pipeline0/GstLibcameraSrc:libcamerasrc0:
Camera.start() failed with error code -32
Execution ended after 0:00:00.013385834
Setting pipeline to NULL ...
Freeing pipeline ...
GMSL lock is not enough, video lock is needed for MIPI CSI2 output. The video lock will only happen in Frame Sync mode when multiple cameras are used.
I trace the driver the error log is:
<7>[ 26.481786] mx95wecam 8-0062: !!!!!! drivers/media/i2c/mx95wecam.c:L302 mx95wecam_get_fmt()
<4>[ 26.481797] !!!!!! drivers/media/mc/mc-entity.c:L875 __media_pipeline_start()
<4>[ 26.481802] Link 'mx95wecam 8-0062':0 -> 'max96724 3-0027':0 is valid
<4>[ 26.481807] !!!!!! drivers/media/mc/mc-entity.c:L897 __media_pipeline_start()
<4>[ 26.481811] Validating pad 'mx95wecam 8-0062':0
<4>[ 26.481815] !!!!!! drivers/media/mc/mc-entity.c:L836 __media_pipeline_start()
<4>[ 26.481819] !!!!!! drivers/media/mc/mc-entity.c:L897 __media_pipeline_start()
<4>[ 26.481824] Validating pad 'max96724 3-0027':1
<4>[ 26.481827] !!!!!! drivers/media/mc/mc-entity.c:L836 __media_pipeline_start()
<4>[ 26.481832] !!!!!! drivers/media/mc/mc-entity.c:L863 __media_pipeline_start()
<7>[ 26.481839] mx95wecam 9-0062: !!!!!! drivers/media/i2c/mx95wecam.c:L302 mx95wecam_get_fmt()
<4>[ 26.481845] Link 'mx95wecam 9-0062':0 -> 'max96724 3-0027':1 failed validation: -32
<4>[ 26.481851] !!!!!! drivers/media/mc/mc-entity.c:L919 __media_pipeline_start()
<4>[ 26.481860] !!!!!! drivers/media/platform/nxp/imx8-isi/imx8-isi-video.c:L1312 mxc_isi_video_streamon()
the link A pipe 0 camera mx95wecam 8-0062 is pipe link ok.
the link B pipe 1 camera mx95wecam 9-0062 is pipe line failed.
That is the pipe set issue?
The default mx95mbcam driver is combined to ox03c10+MAX96717, I think customer should change the code, and what's the dts setting?
yes, I modified the code with imx95-19x19-evk-ox03c10.dtso and mx95mbcam.c.
BTW, when and connected only one camera is ok.
My 95 evk is the A1 version chip, not the B0 version chip.
You can keep the 4 camera setting in dts, but just connect two cameras on port 0 and port 1.