2365080_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2365080_en-US

2365080_en-US

S32E288 Failure during execution of python script

Hi Nxp experts,

I created a new S32E288 M33 project on S32 Design Studio for S32 Platform Version: 3.6.7, then built and try to run it on S32 Debugger,

cszhang_2-1778704023580.pngcszhang_2-1778704023580.png

but i got 

cszhang_4-1778704082217.pngcszhang_4-1778704082217.png

Please help me understand what caused the issue.

Thanks

 
 



 

Re: S32E288 Failure during execution of python script

Hello @cszhang,

Thanks for reaching out to us. About your problem, could you let me know the RTD version your are using? and if you can debug any of the examples?


Thanks. 

Re: S32E288 Failure during execution of python script

The RTD is

cszhang_0-1778766644319.pngcszhang_0-1778766644319.png

and I tested too, got the same issue. Then I clicked the on Debugger tab,  the SIul2 example project did the configuration generation. measured JTAG VTREF value, it's 3.297 V.

cszhang_1-1778766751847.pngcszhang_1-1778766751847.png

cszhang_0-1778767016041.pngcszhang_0-1778767016041.png


the E2 to JTAG connector, has a 33-ohm resistor on board,

cszhang_2-1778766847722.pngcszhang_2-1778766847722.png




Re: S32E288 Failure during execution of python scriptThanks for the quick response, my coworker is looking into hardware, now seems the FS86 PMIC works not well.Re: S32E288 Failure during execution of python script

Hello again @cszhang,

You can check our recommendations for the FS86 in section 3.1 Power supply recommendation of the S32E HW Design Guidelines, also you can see how the S32E EVB is using the FS86 in the Design Files for the S32E288-975EVB.

Note that the design files are missing the schematics pdf, if you require that file please open a private support ticket using the following steps Tutorial for NXP Support Case Portal. If you do so please include the link to this post and my username so that we ensure I handle the ticket, then I can send you the file.


In any case, please let me know if I can help you with anything else.


Re: S32E288 Failure during execution of python script

Hello @cszhang,

Thanks for all the information. I will need to check if S32DS 3.6.7 works with RTD 2.0.1, the official supported version is 3.6.1:

alejandro_e_0-1778812075407.pngalejandro_e_0-1778812075407.png


However, following the AN12530, using 33 ohm resistors is not the best approach, the recommended connections shown in section 7 Example schematics show 0 ohm resistors in series:

alejandro_e_1-1778812231629.pngalejandro_e_1-1778812231629.png

Please try using 0 ohm resistors and let me know if the behavior changes.

If the problem persists, please share the state of the BOOTMOD pins in your board.


Thanks.




Re: S32E288 Failure during execution of python script

Hello again @cszhang,

Were you able to overcome the problem with the PMIC? From my side I was able to debug the Siul2_Dio_Ip_Example_S32Z2XX_SMU sample project in S32DS 3.6.7, using a S32Z280-594EVB. Therefore the software environment should not represent a problem.

In any case, let me know if I can help you with anything else.


Regards. 

Tags (1)
No ratings
Version history
Last update:
‎05-30-2026 03:56 AM
Updated by: