Dear NXP Technical Support Team,
Hello!
BOARD: IMX8MP
Yocto: scarthgap 6.6.23
On the i.MX8mp development board, I encountered this error.
## imx8mp-lpddr4-evk kernel: Internal error: Oops - Undefined instruction: 0000000002000000 [#1] PREEMPT SMP
## imx8mp-lpddr4-evk kernel: Modules linked in: fsl_jr_uio caam_jr caamkeyblob_desc caamhash_desc caamalg_desc crypto_engine authenc libdes crct10dif_ce polyval_ce polyval_generic snd_soc_fsl_asoc_card dw_hdmi_cec snd_soc_fsl_sai snd_soc_fsl_micfil snd_soc_fsl_xcvr imx8_media_dev(C) snd_soc_imx_audmux snd_soc_fsl_aud2htx snd_soc_fsl_easrc snd_soc_fsl_utils snd_soc_fsl_asrc imx_pcm_dma rtc_ds1307 snd_soc_wm8962 caam secvio error imx_dsp_rproc xt_conntrack nf_conntrack nf_defrag_ipv4 iptable_filter fuse
## imx8mp-lpddr4-evk kernel: CPU: 3 PID: 79 Comm: galcore_deamon/ Tainted: G C 6.6.23-lts-next-dirty #1
## imx8mp-lpddr4-evk kernel: Hardware name: YTX FT Release Distro (DT)
## imx8mp-lpddr4-evk kernel: pstate: 60000005 (nZCv daif -PAN -UAO -TCO -DIT -SSBS BTYPE=--)
## imx8mp-lpddr4-evk kernel: pc : dma_fence_signal+0x58/0x64
## imx8mp-lpddr4-evk kernel: lr : gckOS_Signal+0x180/0x244
## imx8mp-lpddr4-evk kernel: sp : ffff800082a6bd00
## imx8mp-lpddr4-evk kernel: x29: ffff800082a6bd10 x28: 0000000000000000 x27: ffff800082a6be10
## imx8mp-lpddr4-evk kernel: x26: 0000000000000000 x25: ffff800081b3c008 x24: ffff000026b7f3c4
## imx8mp-lpddr4-evk kernel: x23: ffff0000d1b6c1e0 x22: ffff0000d0d64044 x21: 0000000000000000
## imx8mp-lpddr4-evk kernel: x20: ffff0000d0d64048 x19: ffff000026b7f3c0 x18: 0000000000000000
## imx8mp-lpddr4-evk kernel: x17: 0000000000000000 x16: 0000000000000000 x15: 0000ffff8db25538
## imx8mp-lpddr4-evk kernel: x14: 0000000000000000 x13: 0000000000000209 x12: 0000000000000002
## imx8mp-lpddr4-evk kernel: x11: 0000000000000040 x10: ffff0000d0d64050 x9 : ffff0000d0d64048
## imx8mp-lpddr4-evk kernel: x8 : ffff000006433b78 x7 : 0000000000000000 x6 : 000002a5fe056003
## imx8mp-lpddr4-evk kernel: x5 : 00ffffffffffffff x4 : ffff0000d1b6c210 x3 : 0000000000000000
## imx8mp-lpddr4-evk kernel: x2 : 0000000000000000 x1 : ffff0000d02b6740 x0 : 0000000000000000
## imx8mp-lpddr4-evk kernel: Call trace:
## imx8mp-lpddr4-evk kernel: dma_fence_signal+0x58/0x64
## imx8mp-lpddr4-evk kernel: gckOS_UserSignal+0x7c/0xb0
## imx8mp-lpddr4-evk kernel: gckEVENT_Notify+0x21c/0x410
## imx8mp-lpddr4-evk kernel: gckHARDWARE_Notify+0x68/0xc8
## imx8mp-lpddr4-evk kernel: gckKERNEL_Notify+0x20/0x2c
## imx8mp-lpddr4-evk kernel: threadRoutine+0x1c/0x78
## imx8mp-lpddr4-evk kernel: kthread+0x110/0x114
## imx8mp-lpddr4-evk kernel: ret_from_fork+0x10/0x20
## imx8mp-lpddr4-evk kernel: Code: 2a1303e0 a94153f3 a8c27bfd d50323bf (d65f03c0)
## imx8mp-lpddr4-evk kernel: ---[ end trace 0000000000000000 ]---According to "dma_fence_signal+0x58/0x64", I checked the "dma_fence_signal" function and found that the instruction corresponding to the 0x58 position is the "ret" instruction.
file path: imx8mp-xwayland/tmp/work-shared/imx8mp-lpddr4-evk/kernel-source/drivers/dma-buf/dma-fence.c
int dma_fence_signal(struct dma_fence *fence)
{
unsigned long flags;
int ret;
bool tmp;
if (!fence)
return -EINVAL;
tmp = dma_fence_begin_signalling();
spin_lock_irqsave(fence->lock, flags);
ret = dma_fence_signal_timestamp_locked(fence, ktime_get());
spin_unlock_irqrestore(fence->lock, flags);
dma_fence_end_signalling(tmp);
return ret;
}
EXPORT_SYMBOL(dma_fence_signal);## aarch64-linux-gnu-objdump -r -d vmlinux | grep -A 30 \:
ffff8000809bcfe8 :
ffff8000809bcfe8: d503233f paciasp
ffff8000809bcfec: a9be7bfd stp x29, x30, [sp, #-32]!
ffff8000809bcff0: 910003fd mov x29, sp
ffff8000809bcff4: a90153f3 stp x19, x20, [sp, #16]
ffff8000809bcff8: b4000260 cbz x0, ffff8000809bd044
ffff8000809bcffc: aa0003f3 mov x19, x0
ffff8000809bd000: f9400000 ldr x0, [x0]
ffff8000809bd004: 942b4fed bl ffff800081490fb8 <_raw_spin_lock_irqsave>
ffff8000809bd008: aa0003f4 mov x20, x0
ffff8000809bd00c: 97dd9d70 bl ffff8000801245cc
ffff8000809bd010: aa0003e1 mov x1, x0
ffff8000809bd014: aa1303e0 mov x0, x19
ffff8000809bd018: 97ffff6e bl ffff8000809bcdd0
ffff8000809bd01c: 2a0003e2 mov w2, w0
ffff8000809bd020: aa1403e1 mov x1, x20
ffff8000809bd024: f9400260 ldr x0, [x19]
ffff8000809bd028: 2a0203f3 mov w19, w2
ffff8000809bd02c: 942b4eb5 bl ffff800081490b00 <_raw_spin_unlock_irqrestore>
ffff8000809bd030: 2a1303e0 mov w0, w19
ffff8000809bd034: a94153f3 ldp x19, x20, [sp, #16]
ffff8000809bd038: a8c27bfd ldp x29, x30, [sp], #32
ffff8000809bd03c: d50323bf autiasp
ffff8000809bd040: d65f03c0 ret
ffff8000809bd044: 128002b3 mov w19, #0xffffffea // #-22
ffff8000809bd048: 17fffffa b ffff8000809bd030 I would like to know why the "ret" instruction is causing the problem? And what should I do to avoid this error? This is an occasional occurrence. I don't yet know what kind of action caused this problem to happen. I am unable to manually reproduce this issue.
Hi @James33
Are you using the standard Linux kernel or PREEMPT Linux?
Best Regards,
Zhiming