2362509_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2362509_en-US

2362509_en-US

How to setup and use the libcamera on the imx8mplus

We need to perform the libcamera software ISP on the imx8mplus board to understand how efficiently it can work. According to official libcamera documents it have the support for the IMX8MP for both hardware ISP and also with ISI. I think from the ISI it is with software ISI. But the documentation/guide to perform this is unclear and very confusing. I am new to libcamera and a lot of confusions on how it works exactly and how it is going to help us in this software ISP part. we have tested the gstreamer bayer2rgb element also, not satisfied with results. 


Our som is imx8mplus & kernel version  6.6.52-compulab-4.1-g94ac18e782b4-dirty.

Thanks and regards 
Vishnu S

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusi.MX 8M | i.MX 8M Mini | i.MX 8M NanoRe: How to setup and use the libcamera on the imx8mplus
Hello,
 
For the implementation of libcamera in our BSP you can refer to chapter 7.3.9 Libcamera in the i.MX Linux User's Guide 
 
Also as reference there is an open source on GitLab  https://gitlab.com/ideasonboard/nxp/libcamera 
Re: How to setup and use the libcamera on the imx8mplus

The correct upstream reference for libcamera is https://gitlab.freedesktop.org/camera/libcamera and has very good support for i.MX8MP or the ISI and SoftISP for the NXP devices without an ISP.

Howveer, on a 6.6 kernel, for libcamera support on i.MX8MP you might need benefit from additional kernel patches which are not in the 6.6 NXP BSP.  We've started https://git.ideasonboard.com/camera/meta-libcamera which can add these patches to the NXP BSP - but it's only been tested on the FRDM-IXM8MP board. We'd be happy to work with anyone to add more platforms to the layer.

You can communicate and ask questions on the matrix channel or join the mailing list for more direct libcamera support:

https://matrix.to/#/#libcamera:matrix.org

https://lists.libcamera.org/listinfo/libcamera-devel


Tags (1)
No ratings
Version history
Last update:
‎07-11-2026 02:28 AM
Updated by: