2362392_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2362392_en-US

2362392_en-US

RGB-IR Camera OX05B1S with i.MX95

Hi

As per i.MX Linux Reference Manual...  Can some one help  how to get SCH-89961 Adapter card. My requirement is to integrate RGB-IR camera with i.MX95. Or any other rgb-ir camera compatible with i.MX95?

akak1_0-1778230986123.png

Regards



Re: RGB-IR Camera OX05B1S with i.MX95

1. OX05B1S + RPI‑CAM‑MINISAS on FRDM i.MX95

Yes, but you also need an FPC cable.
A bare sensor alone is not sufficient.

2. Leopard Imaging LI‑OX05B1S‑MIPI‑137H

Will it work with the existing i.MX95 driver?

Yes — if you use the RAW MIPI output mode, not ISP‑processed output.

3. 5MP RGB‑IR GMSL2 Camera (Jetson AGX Orin type)

Will this work on i.MX95?

No — not directly. Not recommended.

4. Modules with Pre‑integrated ISP
Do I need to disable i.MX95 ISP?

Yes — you must bypass or disable the i.MX95 ISP if the module outputs processed video.

Re: RGB-IR Camera OX05B1S with i.MX95

Hi @yipingwang 
Thank you for quick response. Could you please help with some additional information as requested below.

1. I want to go with OX05B1S sensor, will purchase of sensor and RPI-CAM-MINISAS would be sufficient to integrated to FRDM i.MX95? Do I need FPC cable as well?

2. Will 

LI-OX05B1S-MIPI-137H - Leopard Imaging Inc. this module also work with existing i.MX95 driver?

3. How about 
5MP RGB-IR Global Shutter GMSL2 Camera for NVIDIA Jetson AGX Orin

Leopard as well as e-Consystem Camera module contains pre-integrated ISP, does it mean I need to disable i.MX95 ISP?
Regards

Re: RGB-IR Camera OX05B1S with i.MX95
  • SCH‑89961 Rev.B is an internal NXP camera adapter board.
  • It is explicitly referenced in the i.MX Linux Reference Manual as the MIPI‑CSI adapter used to connect:
    • OmniVision OS08A20
    • OmniVision OX05B1S
  • It is not a commercial product (not sold via Mouser/Digi‑Key).
  • It is used internally by NXP and selected partners for EVK validation.
    You cannot directly buy SCH‑89961.

NXP does not expect customers to use SCH‑89961. Instead, use standard mini‑SAS or FPC MIPI adapters supported by the i.MX95 EVK.

Supported alternatives include:

Adapter

Purpose

RPI‑CAM‑MINISAS

FPC camera → mini‑SAS

IMX‑MIPI‑HDMI

Display/output

IMX‑LVDS‑HDMI

Display/output

  • These are listed in the official i.MX95 Camera Software Pack documentation

RAW MIPI‑CSI RGB‑IR sensors (recommended)

i.MX95 ISP natively supports RGB‑IR fusion.

Best‑known options:

Sensor

Vendor

Notes

OX05B1S

OmniVision

RGB‑IR, officially supported

OS08A20

OmniVision

Uses same driver as OX05B1S

AR0234 RGB‑IR

onsemi

Used in automotive vision

OV2312 RGB‑IR

OmniVision

Global shutter (needs porting)

OS08A20 & OX05B1S work out‑of‑box using the same kernel driver on i.MX95.

Pre‑integrated RGB‑IR camera modules (easier)

Vendors offering ready‑made RGB‑IR cameras with Linux support:

e‑con Systems

  • RGB‑IR camera modules
  • Sensor tuning & ISP support
  • Custom i.MX95 enablement available on request

Examples:

  • OV2312 RGB‑IR
  • AR0830 RGB‑IR
Re: RGB-IR Camera OX05B1S with i.MX95

Hi @yipingwang 

Thank you very much for the clarification.

One more question, is this "22-pin/15-pin camera connector FPC cable"
be available for purchase separately. Internet search results in multiple options hence asking.

Re: RGB-IR Camera OX05B1S with i.MX95

Hi @yipingwang 
Could you please check and respond? I see multiple part number of sensor on Arrow electronics website. Could you please help me identifying exact part number as well as part number of FPC cable..

https://www.arrow.com/en/search-result.html?keyword=ox05b1s&currPage=1

Regards

Re: RGB-IR Camera OX05B1S with i.MX95
Yes, these 22‑pin ↔ 15‑pin FPC (CSI camera) cables are standard and easily available, you can buy them separately without any issue.
Re: RGB-IR Camera OX05B1S with i.MX95

I see few threads related to Camera setup still open in the community. Can someone respond to my question in case you are aware of? Appreciate help...

Re: RGB-IR Camera OX05B1S with i.MX95

Hello @yipingwang and All,
I have not been able to source OX05B1S based FPC camera module that can directly connect with RPI-CAM-MINISAS adapter hence planning to go ahead with

https://leopardimaging.com/product/robotics-cameras/cis-2-mipi-modules/i-pex-mipi-camera-modules/glo...

Since this module does not have in-built ISP, I am assuming I will be able to get same working..
Please provide your input in case you see any major problem with this approach..
















Re: RGB-IR Camera OX05B1S with i.MX95

I am going to conclude that no has tried RGB-IR or IR camera with i.MX93 or i.MX95 although claimed to support as per document.

Tags (1)
No ratings
Version history
Last update:
‎06-26-2026 02:35 AM
Updated by: