2360465_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2360465_en-US

2360465_en-US

Success status of flash.bin flashing

Flashing of flash.bin of flash_spl binary is successfully completing 100% but later flashiong of wic image is not proceding.

Help me in understanding why flash.bin is not rturning done status.

Re: Success status of flash.bin flashing

Hello,

How are you flashing it?

Maybe is not able to move to fastboot, you can confirm it in debug console.

Best regards.

Re: Success status of flash.bin flashing

When i checked for SPL in generated flash.bin below is the content. Help me where could i been wrong

build-wayland/tmp/deploy/images/imx8qxpc0mek$ strings flash.bin | grep -i spl

spl: ERROR: unsupported device
SPL: Unsupported Boot Device!
SPL: failed to boot from all boot devices
U-Boot SPL 2024.04-lf_v2024.04+g6c4545203d1+p0 (Nov 15 2024 - 04:02:13 +0000)
SPL: Image overlaps SPL
SPL: Image too large
spl: unsupported mmc boot device.
spl: could not initialize mmc. error: %d
spl: could not find mmc device %d. error: %d
spl: mmc init failed with error: %d
spl: mmc partition switch failed
spl: mmc: wrong boot mode
display_init
Display the FIPS mode of the SoC by reading fuse 0xA, bit 3
Successfully finished the power up sequence of display.
SPL Phase
TI Keystone SPL Image
TI OMAP SPL With GP CH
sfspl
StarFive SPL Image
display MMC info
u-boot,dm-spl
splashimage=0x9e000000
display-timings
display-subsystem
fsl,imx-display-subsystem
//ldb@562210e0/lvds-channel@0/display-timings/timing0
display0
display1
split_vm_region

Re: Success status of flash.bin flashing

Hello,

The log shows that is not able to find a bootable device.

Are you using a custom image? If yes, what changes did you do?

Are you using the MEK board?

Best regards.

Tags (1)
No ratings
Version history
Last update:
‎05-07-2026 02:30 AM
Updated by: