2360273_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2360273_en-US

2360273_en-US

SafeRTOS_GCC_S32K344_WEB_v9.6.2

I am using SafeRTOS package: SafeRTOS_GCC_S32K344_WEB_v9.6.2

My setup:

  • IDE: S32 Design Studio v3.5
  • Installed RTD: 3.x

Issue:

  • Getting compilation errors (missing headers / driver mismatch)

Observation:

  • This SafeRTOS project seems to be based on RTD 6.x

Questions:

  1. Which exact RTD version is required for this SafeRTOS package?
  2. Is RTD 6.0.0 compatible with S32DS v3.5?
  3. Do I need any additional plugins or updates in S32DS?
  4. Any specific environment variable or path configuration needed?
Re: SafeRTOS_GCC_S32K344_WEB_v9.6.2Thanks for the clarification.
Also is their document like RTD_3_0_0_download_latest_July_2024__only_P07 document for 3.6 software installtion.
Based on your response, I understand that:

RTD 6.0.0 requires S32 Design Studio v3.6.1
My current setup (S32DS v3.5 + RTD 3.x) is not compatible

I will migrate to the recommended environment.

However, I need some guidance regarding correct setup for S32DS v3.6.x:

Could you please confirm the exact installation sequence for:
S32 Design Studio v3.6.1
RTD 6.0.0 (S32K3)
Should RTD be installed via:
S32DS Update Site (Extensions & Updates), or
Manual package installation (offline ZIP method)?
Is there any specific S32DS v3.6.x update (patch version) required to ensure compatibility with RTD 6.0.0?
After installation, are there any additional steps required such as:
SDK path configuration
Environment variables
Toolchain selection
Can you confirm if importing the SafeRTOS project directly will automatically detect RTD 6.0.0, or manual configuration is needed?
Re: SafeRTOS_GCC_S32K344_WEB_v9.6.2

Hi,

Q: Which exact RTD version is required for this SafeRTOS package?
A: SafeRTOS is a 3rd‑party product, so NXP cannot strictly define which RTD version is required. This is primarily a question for the SafeRTOS package developer. If the developer states that the package is based on RTD 6.0.0, then that RTD version should be used.

Q: Is RTD 6.0.0 compatible with S32 Design Studio v3.5?
A: No. RTD 6.0.0 is intended to be used with S32 Design Studio v3.6.1, not v3.5.

Q: Do I need any additional plugins, updates, or special configuration?
A: No. If the SafeRTOS package is based on RTD 6.0.0, then using S32DS v3.6.1 with RTD 6.0.0 installed is sufficient. No additional plugins, environment variables, or special configuration are required.

BR, Petr

Re: SafeRTOS_GCC_S32K344_WEB_v9.6.2

Hi,

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/How-To-Download-Install-and-Configure-... Different RTD version is used in this video, but steps are the same. 
When you import a project into S32DS, the RTD version is not automatically checked.

BR, Petr
标记 (1)
无评分
版本历史
最后更新:
‎05-10-2026 02:43 AM
更新人: