2359914_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2359914_en-US

2359914_en-US

What is the cause of SMC_SC_LOCKED_NOP?

Hello,

when using imx8mp Android 15, the following message appears during startup. What could be causing this?

thanks.


01-01 00:00:02.055 1 1 I init: Loaded kernel module /lib/modules/soc-imx8m.ko will appear when booting
01-01 00:00:02.062 1 1 E : trusty trusty: failed to get version: -1
01-01 00:00:02.062 1 1 I : trusty trusty: selected api version: 0 (requested 5)
01-01 00:00:02.067 83 83 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1
01-01 00:00:02.067 84 84 E : trusty trusty: The message "locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1

01-01 00:00:02.067 85 85 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1

01-01 00:00:02.067 86 86 E : trusty trusty: locked_nop_work_func: SMC_SC_LOCKED_NOP failed -1

01-01 00:00:02.067 1 1 W : trusty trusty: trusty-share not supported on secure side, error=-1" could be causing this problem.

Re: What is the cause of SMC_SC_LOCKED_NOP?

Hi @GavinChen,
Thank you for contacting NXP Support!


Could you please provide more details about the error you are encountering?
I have tested the i.MX8MP EVK using the pre compiled image, and it is working as expected on my side.


Are you using an EVK board?


Best regards,
Chavira

标记 (1)
无评分
版本历史
最后更新:
3 周之前
更新人: