2356873_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2356873_en-US

2356873_en-US

Does LPC1788FBD208K have a chip diagnostic library? If IEC61508 SIL2 or IEC60730/IEC60335 Class B, Functional Safety Certification, cpu needs diagnostic library

Does LPC1788FBD208K have a chip diagnostic library? If IEC61508 SIL2 or IEC60730/IEC60335 Class B, Functional Safety Certification, cpu needs diagnostic library

LPC17xxRe: LPC1788FBD208K 有芯片诊断库吗?如IEC61508 SIL2或IEC60730/IEC60335 Class B,功能安全认证,cpu需要诊断库

Hi @Messi

The LPC1788FBD208K does not have an official, directly supported "Chip Level Diagnostics Library" / Safety Library for IEC 61508 SIL2 or IEC 60730 / IEC 60335 Class B certification.

IEC 60730 Safety Standard for Household Appliances | NXP Semiconductors

BR

Harry.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎04-29-2026 02:33 AM
更新者: