From codewarrior to hardwareI'm using CW_VSPA_v10.3.10. After successfully debugging my code, I don't know how to deploy it to the hardware. The board I'm using is LA1224. I noticed that all the example files include both .eld and .map files, but only the .eld file is generated in my project.
Re: From codewarrior to hardwareThank you. But I'm still wondering whether I can deploy my codes by using codewarrior Tap and how to use it. I tried to write a script but failed, so are there any examples or instructions that can tell me how to write a script?
Re: From codewarrior to hardwareDeploying your code to the LA1224 board
There are two common deployment paths, depending on whether you want RAM loading or persistent Flash loading.
Option A: Load directly to hardware using the debugger (most common during development)
This is usually what you already did when debugging.
Steps:
- Connect the LA1224 board (JTAG / probe / USB as required)
- In CW_VSPA:
Run → Debug Configurations
- Select your VSPA / LA1224 debug configuration
- Make sure:
- The .eld file from your project is selected
- Click Debug
This already deploys your code into target RAM
It is not persistent (power cycle clears it)
Option B: Program the code into Flash (standalone operation)
If you want the LA1224 to boot your application automatically after reset:
Typical process:
- Build the project → obtain
.eld
- Use the LA1224 Flash programming tool (varies by board support package):
- Often launched from CW_VSPA:
Tools → Flash Programmer
or
Run → External Tools
- Select:
- Target: LA1224
- Input file: your
.eld
- Program to Flash
- Reset or power-cycle the board
Code now runs without debugger
.map file is irrelevant here
Re: From codewarrior to hardwareHi, I'm having the same problem. I'm using CodeWarrior for VSPA 10.3.10, but I don't see the “Tools - Flash Programmer” option there.
Under “Target Tasks,” the only options are “Import/Export/Fill Memory” and “HW Diagnostics.”
How can I program the VSPA image to the flash memory?
For the E200, I use the Flash Programmer from CWforARM. I successfully flash *xspi.bin with an offset of 0x0.