2350716_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2350716_en-US

2350716_en-US

UJA1169 can not write Mode control register (0x01) with S32k312

I try to write UJA1169 registers.

As for register Lock control register (Address: 0x0A), it seems OK to write the value I want.

But as for Mode control register (0x01), the register value not change.

The details is like below:

zyt_0-1776163690545.png


What's the different of the write operation of them?How can I successfully write Mode control register?


Re: UJA1169 can not write Mode control register (0x01) with S32k312

I read SBC configuration control register (Address: 0x74) the value is value 0x10. Watchdog status register (0x05) value is 0x01, at the begining.

that seems means SBC is not in Force normal mode.

zyt_0-1776216944823.png


Re: UJA1169 can not write Mode control register (0x01) with S32k312

Hi,

What is the device's operational state? If FNM, the SBC restricts writes to most control registers.

Snímek obrazovky 2026-04-14 162604.png

BRs, Tomas

Tags (1)
No ratings
Version history
Last update:
‎04-15-2026 05:33 AM
Updated by: