Hello Team
May I ask about the S32K3 Crypto version?
Regarding the Crypto module, I have confirmed that it is not included in official releases such as S32K3 RTD 7.0.0 / 7.0.1,
and that it exists only as Code Drop releases such as 7.0.0_P01 and 7.0.1_P02.
Since Code Drops cannot be applied to mass production, I have a question from a customer regarding mass production use.
Would it be acceptable to mix RTD 4.4.0 Crypto (or another existing version) with RTD 7.0.0 or 7.0.1 without issues?
Thank you.
Hi @Luke_Chun
Would you mind taking 2 minutes to complete this feedback form?
Software Support Case Feedback Survey – Prefilled form
It would help us to have better support next time.
Hi @Luke_Chun
If customer want to use in mass production, they have to wait until an official standard release
(EAR, PRC or RFP) like mentioned in Release Notes.
I see that RTD 7.0.0 or 7.0.1 supporting ASR 23-11, not 4.4. Furthermore, each Crypto release was tested on an RTD version, in this case is 7.0.0 and 7.0.1.
So, we cannot guarantee it works with RTD 4.4.0 Crypto.