2346849_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2346849_en-US

2346849_en-US

Configuring sja1105p using sja1105-tool failed on the custom board.

We used a customized version of imx8mp-evk to connect the eth1 eqos to port2 of the sja1105p via RGMII, and the other ports were also directly connected to the SoC's MAC address via RGMII. After downloading our bin configuration file using sja1105-tool, we were unable to ping the device. The Rx value on eth1 remained at 0 and did not increase, while the Tx value was increasing, as if the data was not reaching the switch.

eth1: flags=4163  mtu 1500
        inet 172.24.172.100  netmask 255.255.255.0  broadcast 0.0.0.0
        inet6 fe80::a4c1:7eff:feda:f448  prefixlen 64  scopeid 0x20
        ether a6:c1:7e:da:f4:48  txqueuelen 1000  (Ethernet)
        RX packets 0  bytes 0 (0.0 B)
        RX errors 0  dropped 0  overruns 0  frame 0
        TX packets 38  bytes 4332 (4.2 KiB)
        TX errors 0  dropped 0 overruns 0  carrier 0  collisions 0
        device interrupt 212  

We placed the bin file in /lib/firmware, and the conf file also follows the official configuration. We used the command sja1105-tool config upload to download the file.





i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusRe: Configuring sja1105p using sja1105-tool failed on the custom board.

@JosephAtNXP Thank you for your reply. Sure, The attachment contains the DTS and schematic diagram. I've tried the configurations in lines 211-215 and 318-329 of the DTS file; lines 227-316 are the official EVK configuration.

 

PixPin_2026-04-09_09-21-12.pngPixPin_2026-04-09_09-22-20.pngPixPin_2026-04-09_09-23-42.png

Re: Configuring sja1105p using sja1105-tool failed on the custom board.

Hi,

Thank you for your interest in NXP Semiconductor products,

Could you please share your schematics and DTS configuration?

Regards

Re: Configuring sja1105p using sja1105-tool failed on the custom board.

The attachment is our configuration script.

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎04-09-2026 02:34 AM
更新者: