MCF5480 boot debug errori repaired a MCF5480 board,while booting,i meet some UART error. i want to know,if this error caused by hardware damage?


Boot ROM|Booting | FlashRe: MCF5480 boot debug errorThe MCF5480 and DSP worked correctly everbefore.I didn't change anything about hardware or software. While VFP software displayed "Dual Port RAM Uninitialized".
As you mean,how to change DSP's program?
Re: MCF5480 boot debug errorHello,
Yes, Change the configuration in the DSP.
Regards
Re: MCF5480 boot debug errorHello,
The error "RTS 200100 was not 0" in ColdFire processors indicates a critical communication failure between the debugger and the chip. This code is often tied to "invalid parameters" or a synchronization mismatch during the flash programming or erase process .
Key Causes and Solutions
- Debugger Driver Incompatibility: This is the most common cause. Using older versions of CodeWarrior on modern operating systems (Windows 10/11) often causes driver conflicts with the P&E Multilink interface .
- Solution: Install the latest P&E Micro drivers or run your development environment in a Windows XP/7 Virtual Machine.
- Target Initialization Issues: The target initialization file (often a
.tcl or .cfg script) might contain incorrect parameters for the flash base address, bank size, or clock settings (PLL) .
- Solution: Verify that the flash base address and memory map in your project settings match your specific ColdFire model Enable "Verify Target Memory Writes" in the Target Configuration to check if the algorithm downloads correctly .
- USB Port Speed Issues: High-speed USB 3.0 ports can sometimes be too fast for older BDM/JTAG debuggers, leading to timing errors .
- Solution: Connect the debugger through a powered USB 2.0 hub or try a different USB port on your machine.
- Hardware Interference: Improper hardware connections or interference on the BDM lines can trigger communication losses .
- Solution: Check for cold solder joints on the BDM header and ensure you are not using an excessively long ribbon cable.
Debugging Steps
- Check for duplicate processes: Open Task Manager and ensure there isn't another instance of
pegdbserver_console or the debugger running .
- Verify the Hardware ID: Ensure the hardware selected in the NXP Community or IDE matches the physical chip on your board (e.g., ColdFire V1 vs V2) .
- Power Cycle: Completely power down both the target board and the debugger to reset the communication interface.
Regards
Re: MCF5480 boot debug errorThanks for your reply.This error occured between MCF5480 and a DSP chip .They communicated through UART3,While system init, RTS and CTS signals reported error.This snap picture's messages obtained from the debug UART Port. Did this error caused by a hardware fault?