Does NXP publish BSDL files for JTAG boundary scan for the RW61x? I can't seem to find them.
Hello,
Hope you are doing well. Are you using RTOS or Zephyr?
Also, could you please clarify if you are working with a module?
Regards,
Ricardo
I'm not sure why OS would have anything to do with boundary scan files.
I'm using Zephyr 4.4.0.
Module is from u-blox, but has an RW610 on it.
Hello,
Could you please clarify which chip package are you using? BGA/QFN or CSP?
Best Regards,
Ricardo
Hello, I am also looking for the BSDL file for the rw61x series chips.
Can you please point me in the right direction to be able to download these files?
Thanks,
Alex
Could someone from NXP actually answer this question??
Is there a BSDL file for the RW61x and if so where can we download it?
Thanks,
Alex Titsworth