2343829_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2343829_en-US

2343829_en-US

MCXN947: Is there a "1588_EVENT_IN" pin available?

Hello @Harry_Zhang

is there a "1588_EVENT_IN" pin available?

I want to synchronize the internal 1588 timer to e.g. an external GPS PPS signal. Therefore, I need a input pin which capture the signal and store the 1588 counter.

In case of a RT1170, I can found e.g. “ENET_1588_EVENT0_IN” pin. But I can not found such a pin for the N947.

Best regards,
Michael

MCXNRe: MCXN947: Is there a "1588_EVENT_IN" pin available?

Hello @michael_fischer ,

Thanks for your port.

No, the MCXN947 does not provide an external 1588 event input pin.

Hope it helps.

BR

Celeste


Re: MCXN947: Is there a "1588_EVENT_IN" pin available?

Hello @Celeste_Liu 

It's a pity that such a pin is not available. I thought I had just overlooked it. Then I have to think of something else here for synchronization to a GPS PPS signal.

Plan B is to add both signals to inputs from the CTIMER and thus determine the time difference.

Best regards,
Michael

Tags (1)
No ratings
Version history
Last update:
‎04-04-2026 03:26 AM
Updated by: