feasibility for S32N7 update of a cohort image in independentlyHi team,
Schaeffler needs to evaluate and test the OTA use case.
This means that an OTA update should be performed for one cohort and observe that this cohort can be updated independently from the others and also while the other ones are in running mode.
The current AP software does not support the OTA feature. But the OTA is an important topic for all customers.
do we have a document to describe how the FSS supports the OTA feature?
Is it possible to implement this scenario for the customer's proposal ?
FSS_FWRe: feasibility for S32N7 update of a cohort image in independentlyHello, Raoul
Please see the required information as follow:
- Project Name*: Schaeffler S32N79 project
- Customer Contact Point* (Name & Email): [email protected] (FAE)
- Software & Hardware Information: S32N79
- SW Package Info*: FSS-FW/S32N7 RTD/GrayVIP
- SW Version*: FSS-FW 1.18.0/S32N7 RTD 2.0.0 /GrayVIP 1.0.5.3
Re: feasibility for S32N7 update of a cohort image in independentlyHi @Yu_Song.,
The team has been made aware and I'll get back soon with an answer from them.
In the meantime make sure to provide the following information:
- BSSM Contract: Yes / No
- Project Name*:
- Customer Contact Point* (Name & Email):
- Software & Hardware Information:
- SW Package Info*:
- HW* (Board/Chipset/Platform):
- SW Version*:
*required
Thanks a lot,
Raoul
Re: feasibility for S32N7 update of a cohort image in independentlyHi Raoul,
any feedback?
BR,
Yu
Re: feasibility for S32N7 update of a cohort image in independentlyHi Yu,
You have received an email from Mircea Ionica with more information.
If you have more questions please ask. If the email response is satisfactory, please mark this message as solution for this post.
Tanks,
RaoulRe: feasibility for S32N7 update of a cohort image in independentlyunderstand the case and thanks very much