Hi Team,
I am currently working with the PN7462 NFC MCU and using the API phhalSysSer_GetDieID() to retrieve the 16-byte Die ID.
I am able to successfully read the Die ID, for example:
00 00 00 00 00 01 7C 0A 39 0A 91 4E 90 36 10 04
I would like to understand more about the internal structure and meaning of these 16 bytes.
Specifically:
Thanks and best regards,
Uday Gowda
Hi Fabian,
Thanks for reply.
Hello sir,
Unfortunately, we don't have a document that provides a bit-map or the structure of the Die ID. Since it can be used as a constant value for each IC the structure isn't disclosed.