I am setting up for the environment of #S32K344
Based on #S32DS 3.5 & RTD 3.0.0
But I can't find the profit #FS26 package
I have tried FS26 package version 2.0.0/3.0.0/4.0.0/5.0.0
All Failed .
Please help or give an advise
Dear @Robin_Shen
Thanks for your support.
I uninstall FS26 packages and tried again to install with your guidance.
but same result.
Please uninstall FS26 S32K3XX 4.0.0 and then reinstall FS26 S32K3XX 2.0.1.
Thanks @Robin_Shen
- S32DS Ver 3.5 240924(update 14)
- NXP GCC for Arm ... build 1728
- RTD ver 3.0.0 P07
with this environment, I have tried to install [SW32K3_RS26_R21-11_2.0.1_D2507].
but FS26 S32K3XX 4.0.0 is automatically installed.
And the result of Example code[Sbc_fs26_example_IP_S32K344] shows 15 ERRORs
Hi
Do you absolutely need to use such an old version as S32K3 RTD 3.0.0? It has now been updated to S32K3 RTD 7.0.0, which has fixed known bugs.
If so, I see the following FS26 SBC RTD is based on S32K3 RTD 3.0.0 P07:
FS26 SBC AUTOSAR R21-11 Version 2.0.1
FS26 SBC AUTOSAR R21-11 version 2.0.0
I'm not sure if the "S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices(3.5.0_D2303): SW32K3xx_..." which S32K3 RTD 3.0.0 depends on is still available for download. If not, I suggest installing S32K3 RTD 3.0.0 through S32DS Extensions and Updates in the latest S32DS v3.6.x. However, please note that you need to install NXP GCC for Arm Embedded Processors v10.2 build 1728.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "ACCEPT AS SOLUTION" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Do you absolutely need to use such an old version as S32K3 RTD 3.0.0? S32DS v3.5 and it's Update/Development package is probably no longer available for download from www.nxp.com for new users.
If you insist on using such an old version, please wait for me to install S32DS v3.5 using the Update/Development Package you can find. Then try installing SW32K3_FS26_R21-11_2.0.1_D2508_DesignStudio_updatesite.zip to see if the problem you are encountering is reproduced.
If you only want to learn about FS26 SBC, then I suggest you install the new SBC FS26 R23-11 6.0.0 + S32K3_S32M27x Real-Time Drivers AUTOSAR R23-11 Version 7.0.0 in S32DS v3.6.6.
Please install SW32K3_RTD_R21-11_3.0.0_P07_D2306_DS_updatesite.zip in S32DSv3.6.6. Then install SW32K3_FS26_R21-11_2.0.0_D2508_DesignStudio_updatesite.zip.
Dear @Robin_Shen
- If you insist on using such an old version
-> YES.
Please check if the FS26 is available with RTD 3.0.0.