2335285_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2335285_en-US

2335285_en-US

NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

I have downloaded the FreeRTOS_10_5_1_3_1_0.zip and I tried to install but the following message appears: 

Artifact not found: jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/features/com.nxp.FreeRTOS.S32K3.3.1.0.feature_3.1.0.202304240736.jar.
jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/features/com.nxp.FreeRTOS.S32K3.3.1.0.feature_3.1.0.202304240736.jar
Artifact not found: jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/binary/com.nxp.FreeRTOS.S32K3.3.1.0.win32.win32.x86_64_3.1.0.202304240736.
jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/binary/com.nxp.FreeRTOS.S32K3.3.1.0.win32.win32.x86_64_3.1.0.202304240736
Artifact not found: jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/features/com.nxp.FreeRTOS.S32K3.root.3.1.0.feature_3.1.0.202304240736.jar.
jar:file:/C:/Users/j.pineiro/MyNXP_Extensions/FreeRTOS_10_5_1_3_1_0.zip!/features/com.nxp.FreeRTOS.S32K3.root.3.1.0.feature_3.1.0.202304240736.jar

I am using S32DS studio v3.5 but I cannot find the files mentioned in the readme: 

Service Pack 1(com.nxp.s32ds.sp1.s32k3xx.update_3.5.0.20230307163114.zip), S32M27x_SP2_CD(SW32M2xx_S32DS_3.5.0_D2302.zip)

Could someone tell me if the origin of the error is related with this? Or I am missing somthing else?

Thank you, regards

Re: NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

Hi @JosePineiro,

That specific FreeRTOS package needs the following dependencies:

  • Make sure S32 Design Studio v3.5, S32 Design Studio for S32 Platform v.3.5 with S32K3 Service Pack 1(com.nxp.s32ds.sp1.s32k3xx.update_3.5.0.20230307163114.zip), S32M27x_SP2_CD(SW32M2xx_S32DS_3.5.0_D2302.zip) and S32K3 RTD 3.0.0 package are installed before this FreeRTOS package.
  • The S32K3 RTD update for Design Studio must be installed as the following steps:
    • Open Help -> S32DS Extensions and Updates. From the next windows, select "S32K3 Real-Time Drivers AUTOSAR 4.4 R21-11 Version 3.0.0" and click Install/Update
  • The FreeRTOS update for Design Studio must be installed as the following steps:
    • Open Window -> Preferences. From the next windows, select S32 Design Studio for S32 Platform -> S32DS Extensions and Updates, click Add All and select the zip archive containing the FreeRTOS update.
  • Open Help -> S32DS Extensions and Updates. From the next windows, select "FreeRTOS for S32K3 3.1.0" then click Install/Update.

I believe the service pack refers to S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices .

Best regards,
Julián

Re: NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

Hi @JosePineiro,

As I've mentioned, the FreeRTOS package also asks for S32K3 Service Pack. Could you try downloading it? S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices.

In order to access the link, you must be logged both into nxp.com and flexera portal.

Best regards,
Julián

Re: NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

Hello @Julián_AragónM, thank you for support me with this topic.

I already have installed RTD 3.0.0:

 

Snipaste_2026-03-20_08-54-42.pngSnipaste_2026-03-20_08-54-42.png

 and also I´m using S32DS v3.5

Snipaste_2026-03-20_08-55-54.pngSnipaste_2026-03-20_08-55-54.png

I follow the steps to install FreeRTOS_10_5_1_3_1_0: windows ->preferences-> add all and select the zip. Then from help ->extension and updates, searching for freeRTOS I try to install but the same error appears 

Snipaste_2026-03-20_08-59-02.pngSnipaste_2026-03-20_08-59-02.png

 any thoughts or missing steps?


thank you so much.

Best regards


Re: NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

Hi @JosePineiro,

You can try accessing the package directly.

From your NXP profile, go into: "Apps and Services > Software Licensing and Support > Software accounts"

This should take you to your available Product List.

From here, scroll down and find "NXP Software > Automotive SW - S32K3 - S32 Design Studio"

There, inside the "Previous" tab, you should be able to see the package named 3.5.0_D2303 S32 Design Studio 3.5.0 Development Package with support for S32K3xx devices.

Please keep in mind that this process is somewhat tedious because you are downloading a previous (outdated) version of the FreeRTOS package. Latest release (SW32K3 FreeRTOS version 7.0.0 CD1) works with latest RTD package version 7.0.0, and S32DS 3.6.6.

Best regards,
Julián

Re: NXP RTOS FreeRTOS_10_5_1_3_1_0 for S32k344

I am logged in nxp.com and I have created an account into Flexera Community | Home but the link still takes me to my profile

Tags (1)
No ratings
Version history
Last update:
‎03-26-2026 02:36 AM
Updated by: