2334329_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2334329_en-US

2334329_en-US

i.MX95 EVK (19x19) – No M7 output when running FlexSPI octal polling example

Hello NXP Support Team,

I am working with an i.MX95 19x19 LPDDR5 EVK and would like some guidance on running an M7 FlexSPI example on real hardware.
Setup and current status

Board: i.MX95 19x19 LPDDR5 EVK
Yocto: latest BSP (Linux 6.12.34, BSP 2.2.0)
Boot media: WIC image flashed to hardware
Cores:
M33 (SM): runs correctly
A55 (Linux): boots and runs correctly
M7: works when using the default power-mode-switch example

Using the standard Yocto WIC image, the following M7 firmware runs as expected:
imx95-19x19-evk_m7_TCM_power_mode_switch.bin

What I attempted

I wanted to try the MCUXpresso SDK M7 example:

FlexSPI Octal Polling Transfer (CM7):
https://mcuxpresso.nxp.com/mcuxsdk/latest/html/examples/driver_examples/flexspi/octal/polling_transf...

To test this on hardware, I replaced the default M7 binary in the Yocto deploy directory:
````
cp flexspi_octal_polling_transfer_cm7.bin \
build-imx95evk/tmp/deploy/images/imx95evk/mcore-demos/imx95-19x19-evk_m7_TCM_power_mode_switch.bin

```

I then rebuilt the WIC image and flashed it to the board.
Observed behavior

M33 and A55 still boot and run correctly
No output on the M7 UART
No visible indication that the M7 example is running

Questions

Is this approach of replacing the M7 binary in the Yocto WIC image valid for running an M7 SDK example?
Does the FlexSPI Octal Polling Transfer example require:
A specific memory placement (e.g., OCRAM vs TCM)?
A specific boot or power configuration that differs from the power mode switch example?
Is additional configuration needed in Yocto or device tree to support this example?
What is the recommended way to flash and run an M7 SDK example on i.MX95 EVK when no debug probe is available?
Are there known limitations or prerequisites for running FlexSPI examples on i.MX95 when Linux and M33 are also active?

Any guidance on the correct and supported flow for running M7 standalone examples on i.MX95 alongside Linux would be greatly appreciated.

Thank you for your support.



Re: i.MX95 EVK (19x19) – No M7 output when running FlexSPI octal polling example

Thanks for the reply,

I have updated the build-imx95evk/tmp/work/imx95evk-poky-linux/imx-system-manager/2025q4/git/configs/mx95evk.cfg and rebuilt and tried booting from the new wic image.


I still don't see anything on the M7 UART terminal (I can see SM output and Linux booting on other two terminals)


Is my approach of loading the M7 binary correct?


Best Regards

Sami

Re: i.MX95 EVK (19x19) – No M7 output when running FlexSPI octal polling example

Hi @s153022 

The previous modifications are based on rpmsg variant. You need to modify configs/mx95evk.cfg if you are not using rpmsg variant.


Best Regards,
Zhiming

Re: i.MX95 EVK (19x19) – No M7 output when running FlexSPI octal polling example

Thanks for your reply.
I have updated the following configuration file:
build-imx95evk/tmp/work/imx95evk-poky-linux/imx-system-manager/2025q4/git/configs/other/mx95evkrpmsg.cfg.
I have also copied flexspi_octal_polling_transfer_cm7.bin and overwritten the following three files:

tmp/work/imx95evk-poky-linux/imx-boot/1.0/git/iMX95/m7_image.bin
tmp/deploy/images/imx95evk/imx-boot-tools/imx95-19x19-evk_m7_TCM_power_mode_switch.bin
tmp/deploy/images/imx95evk/mcore-demos/imx95-19x19-evk_m7_TCM_power_mode_switch.bin

After that, I rebuilt the WIC image using:

bitbake fsl-image-full


When booting from the SD card. I can see the System Manager and Linux booting on two terminals.

However , there is no output from the M7 on the third terminal.


Best Regards

Re: i.MX95 EVK (19x19) – No M7 output when running FlexSPI octal polling example

Hi @s153022 

You need to move FLEXSPI1 from A55 to M7 in system manager.

image.png


Here is mofications based on i.MX95EVK rpmsg variant in imx-sm.

diff --git a/configs/other/mx95evkrpmsg.cfg b/configs/other/mx95evkrpmsg.cfg
index 079a887..9c01028 100755
--- a/configs/other/mx95evkrpmsg.cfg
+++ b/configs/other/mx95evkrpmsg.cfg
@@ -440,12 +440,26 @@ SYSCTR_RD           READONLY
 TSTMR2              OWNER
 V2X_SHE1            OWNER
 WDOG5               OWNER
+FLEXSPI1            OWNER
 
 # Pins
 
 # LPUART3 pins
 PIN_GPIO_IO14       OWNER
 PIN_GPIO_IO15       OWNER
+PIN_XSPI1_DATA0      OWNER
+PIN_XSPI1_DATA1      OWNER
+PIN_XSPI1_DATA2      OWNER
+PIN_XSPI1_DATA3      OWNER
+PIN_XSPI1_DATA4      OWNER
+PIN_XSPI1_DATA5      OWNER
+PIN_XSPI1_DATA6      OWNER
+PIN_XSPI1_DATA7      OWNER
+PIN_XSPI1_DQS        OWNER
+PIN_XSPI1_SCLK       OWNER
+PIN_XSPI1_SS0_B      OWNER
+PIN_XSPI1_SS1_B      OWNER
+
 
 # SAI3 pins
 PIN_GPIO_IO16       OWNER
@@ -473,6 +487,7 @@ PIN_I2C2_SCL         OWNER
 PIN_I2C2_SDA         OWNER
 # Memory
 
+FLEXSPI1_MEM        EXEC, begin=0x000000000, end=0x0FFFFFFFF
 M7MIX               DATA, begin=0x020380000, end=0x02047FFFF
 M7MIX               DATA, begin=0x04A060000, end=0x04A09FFFF
 DDR                 EXEC, begin=0x080000000, end=0x089FFFFFF
@@ -730,7 +745,7 @@ EDMA3_CH60_61       OWNER
 EDMA3_CH62_63       OWNER
 FLEXIO1             OWNER
 FLEXIO2             OWNER
-FLEXSPI1            OWNER
+// FLEXSPI1            OWNER
 FSB                 READONLY
 GIC                 OWNER
 GPIO2               OWNER
@@ -994,22 +1009,22 @@ PIN_SD3_DATA2        OWNER
 PIN_SD3_DATA3        OWNER
 PIN_UART1_RXD        OWNER, test
 PIN_UART1_TXD        OWNER
-PIN_XSPI1_DATA0      OWNER
-PIN_XSPI1_DATA1      OWNER
-PIN_XSPI1_DATA2      OWNER
-PIN_XSPI1_DATA3      OWNER
-PIN_XSPI1_DATA4      OWNER
-PIN_XSPI1_DATA5      OWNER
-PIN_XSPI1_DATA6      OWNER
-PIN_XSPI1_DATA7      OWNER
-PIN_XSPI1_DQS        OWNER
-PIN_XSPI1_SCLK       OWNER
-PIN_XSPI1_SS0_B      OWNER
-PIN_XSPI1_SS1_B      OWNER
+// PIN_XSPI1_DATA0      OWNER
+// PIN_XSPI1_DATA1      OWNER
+// PIN_XSPI1_DATA2      OWNER
+// PIN_XSPI1_DATA3      OWNER
+// PIN_XSPI1_DATA4      OWNER
+// PIN_XSPI1_DATA5      OWNER
+// PIN_XSPI1_DATA6      OWNER
+// PIN_XSPI1_DATA7      OWNER
+// PIN_XSPI1_DQS        OWNER
+// PIN_XSPI1_SCLK       OWNER
+// PIN_XSPI1_SS0_B      OWNER
+// PIN_XSPI1_SS1_B      OWNER
 
 # Memory
 
-FLEXSPI1_MEM        EXEC, begin=0x000000000, end=0x0FFFFFFFF
+// FLEXSPI1_MEM        EXEC, begin=0x000000000, end=0x0FFFFFFFF
 OCRAM_C             EXEC, begin=0x001000000, end=0x001017FFF
 OCRAM               EXEC, begin=0x0204C0000, size=96K
 GPU                 DATA, begin=0x04D900000, end=0x04DD7FFFF
 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎03-19-2026 02:33 AM
更新者: