2334089_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2334089_en-US

2334089_en-US

Unlisted MCU-Link probe

Hello, 

I'm currently trying to setup my MCU-Link probe. 

But it dosen' show up in the MCUxpresso IDE. 

When i try to update the MCU-Link via LinkServer the probe is unlisted (jumpers are open an the LED is off).

Screenshot 2026-03-16 152610.png

When i try to update via ISP (J3 is closed and the LED is red) the MCU-Link is not found. 

Screenshot 2026-03-17 140021.png

Is there any other way to update the MCU Link?

@ErichStyger MCU-LINK 

Re: Unlisted MCU-Link probe

Hello,

Could you help us confirm that when installing the Linkserver, you select "Associate with existing MCUXpresso IDE installations" and associate the  MCUXpresso IDE installations, please refer to photos.

Associate MCUXpresso IDE installations_LinkServer Installation setup.png


Associate MCUXpresso IDE installations_LinkServer Installation setup 2.png


Could you help us share what it shows your device manager for the debugger?

Probably you need to update your MCU-Link driver. Please help us following these steps:

  • With J3 open in MCU-Link probe.
  • In device Manager, Right Click on the debugger and select "update driver"
  • Select "Browse my computer for drivers" and search for the driver in the location: "C:\nxp\LinkServer_25.12.83\MCU-LINK_installer\drivers:"
  • After updating the driver, please retry to update the debugger via ISP mode (with J3 closed) by running "program_CMSIS.cmd" script in [C:\nxp\LinkServer_25.12.83\MCU-LINK_installer\scripts]

Please let me know if that work for you.

Best Regards, Luis

Re: Unlisted MCU-Link probe
 

Hello Luis,

I reinstalled my LinkServer 25.12.83 to make sure that the right boxes are checked.

However after updating the driver again, i still couldn't update the MCU LInk via ISP.

Here is a Picture of the Devicemanger for the Link in ISP Mode

Screenshot 2026-03-19 074647.png

 And one in normal Mode

Screenshot 2026-03-19 075041.png


Re: Unlisted MCU-Link probe

Hello,

There is a method for update using Link Server without the jumper for entering ISP

Jumper-less Update with Linkserver


Could you help us trying this method:

  • Open in cmd the LinkServer path location:
  • Enter the command: "LinkServer probe #1 update auto"

Please let me know if that work for you.

Also, could you help us confirm which firmware version you have currently?

Best Regards, Luis

Re: Unlisted MCU-Link probeHello,

since my MCU Link is flagged as unlisted i'm unable to update via LinkServer. I also tried #0 udate auto and #update auto and update auto.

I have no way to update the MCU Link and i would like to know why. Clearly the problem with "unlisted MCU Link" must have happend before. I can't be that NXP doesn't know how it can happen that the MCU Link is unlisted and not able to be updated.
Re: Unlisted MCU-Link probe

Hi @Ebner ,

I had such an 'unlisted' probe in one case where I had accidentally set the 'SWD disable' jumper. 

Can you check this?

See https://mcuoneclipse.com/wp-content/uploads/2020/11/mcu-link-board-top-side.jpg

I hope this help,

Erich

Re: Unlisted MCU-Link probe

Hello Erich,

Thank you for your reply.

There is no Jumper at J5. And i measured if ther is a shortcut inside the PCB between the two pins. There is none. 

Medien (25).jpg


We tested it on the PC of an colleague an there was the same behaiver.


Re: Unlisted MCU-Link probe

Ok, I believe it might be a problem with your host OS caching mechanism.

Could you follow the extra steps below which collect some extra information which could be helpful to pinpoint the problem?

The process is the following:

a) dump some registry keys so I can see what are your current values. Please provide these values.

b) next, apply a workaround which forces a USB device enumeration

c) run again a script to dump the new registry file content. Please provide that information.



Step a):

I have attached some registry keys in the attached paths.txt file. Save the file locally, then execute the command below to export registry content:

for /f "usebackq delims=" %P in ("paths.txt") do reg query "%P" /s >> reg_dump_before.txt

This exports some registry keys to that reg_dump_before.txt for diagnostics. It would be great if you could share that content.


Step b):

run the following to force a re-enumeration:

  • Have the probe unplugged
  • Set jumper for VCOM disabled. On the MCU-Link this is J4 or the middle jumper)
  • Plug-in probe to PC
  • Remove jumper for VCOM disabled (so enable back VCOM)
  • Re-plug the probe to PC

This forces Windows to re-enumerate the USB device with the current configuration and  hopefully solves the problem.

Step c):

it would be very helpful to see that are the registry keys after that. So can you run the following line to export the values to a different file:

for /f "usebackq delims=" %P in ("paths.txt") do reg query "%P" /s >> reg_dump_after.txt

Then it would be very helpful if you could provide the content too.


I hope this help,

Erich

Re: Unlisted MCU-Link probe

Hello,

Thank you for help.

Unfortunatly it didn't solve the Problem.

Attached are the dump filed before and after. 

I hope this brings you closer to the solution. 


Re: Unlisted MCU-Link probe

Hi @Ebner,

Somehow community notifications did not work for me, seeing the log files only now :-(.

Erich

标记 (1)
无评分
版本历史
最后更新:
‎05-11-2026 02:31 AM
更新人: