2332937_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2332937_en-US

2332937_en-US

2.5G SGMII connected to LX2162A

Hi,

we need to connect 2.5G SGMII interface to LX2162A processor. Is it possbile directly?

In LX2162A reference manual is written that it supports only 1G SGMII however there is USXGMII interface with 2.5G bouadrate. Is it possible to connect 2.5G SGMII to 2.5G USXGMII directly?


Kind regards!


Re: 2.5G SGMII connected to LX2162A

USXGMII and 2.5G SGMII are not directly compatible because they are designed for different Ethernet speeds and use different encoding schemes.

To support 2.5Gbps device to LX2162A, an external PHY that converts 2.5G with the line-side interface to USXGMII is required.

Thanks

Tags (1)
No ratings
Version history
Last update:
‎03-20-2026 03:25 AM
Updated by: