2330347_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2330347_en-US

2330347_en-US

RT1062 ENC module

Dear supporter,
I use RT1062 to realize the ENC function.
Can pin GPIO_SPI_B1_00~GPIO_SPI_B1_07 be configured as the PhaseA or PhaseB input?
If not, can pin GPIO_AD_B0_08~GPIO_AD_B0_11 be configured as the PhaseA or PhaseB input?
Thanks a lot.

Board DesignDevelopment BoardRe: RT1062 ENC module

Hi @lewu1 ,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.

Q1:Can pin GPIO_SPI_B1_00~GPIO_SPI_B1_07 be configured as the PhaseA or PhaseB input?

A1: I double checked pin GPIO_SPI_B1_00~GPIO_SPI_B1_07, and I don't believe these pins can be configured as the PhaseA or PhaseB input.

Q2: If not, can pin GPIO_AD_B0_08~GPIO_AD_B0_11 be configured as the PhaseA or PhaseB input?

A2:  Yes, GPIO_AD_B0_08~GPIO_AD_B0_11  pins can be configured as the PhaseA or PhaseB input.

For your better understanding, I post some figs for you.

Snipaste_2026-03-17_17-09-47.pngSnipaste_2026-03-17_17-09-19.png




Wish it helps you

Best Regards

MayLiu

Re: RT1062 ENC module

You are welcome.

If my post answer your question, please press "Accept as solution".

Best Regards

Re: RT1062 ENC module

Thank you.

Tags (1)
No ratings
Version history
Last update:
‎04-15-2026 03:32 AM
Updated by: