2326392_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2326392_en-US

2326392_en-US

CodeWarror

Does anyone know where I can download a copy of CodeWarrior for 8-bit processors that will run under Linux (Ubuntu)? A general enquiry showed that C/W does run under linux, but all of the links are for windows.

Re: CodeWarror

Hello,

Sorry for the inconveniences, the available version of CodeWarrior for 8-bit processors [CodeWarrior v11.1] is not available for Linux only windows.

Best Regards, Luis

Re: CodeWarror

I know that! I have been using CW for "many years", running under Windows 7 which is running under Dropbox which is running under OSX on my Intel-based MAC. All I want is to do the same thing on my new ARM-based MAC. So far I have installed Dropbox and loaded Windows 11. (earlier versions of Windows are not compatible with the new MACs). I have installed CW 11.1 in Windows and it works.

As I said in my original post CW does not recognise the Multilik debug probe because there is no device driver installed. Please refer to my original post for details of what is required 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎08-08-2026 02:33 AM
更新者: