Hello, currently I want to use the ls1028ardb development board to develop a terminal network card device for the TSN network. All the ls1028ardb images have been successfully built automatically on Ubuntu using flexbuild by running the command "bld -m ls1028ardb". Additionally, the "UG10143 User Guide" has been reviewed.
I would like to ask: To develop a TSN network card device, the QBV and IEEE 802.1AS protocols need to be used. Where can I download the corresponding development routines? Where can I find the documentation introducing the corresponding APIs? How should the project be set up?
The attached is LSDK 21.08, please install and build it on Ubuntu 20.04 Linux PC.
Please refer to "4.3 How to build LSDK with Flexbuild" to build images.
Please refer to "4.1.2 Download and deploy LSDK images with flex-installer in Linux environment" to deploy images on the target board.
Please download "LSDKUG_Rev21.08.pdf" then refer to section "8.8 Time Sensitive Networking (TSN)".