Hello, I am trying to perform DDR configuration on u-boot for the T1042. For this, I need the QCVS 4.5.x version that works on CodeWarrior 10.5.1. I couldn't find it on NXP's official website. I found threads on the forum from people having similar problems, but the links are invalid because the topics are quite old. Could you please share the offline installer for QCVS 4.5.x with me?
dear @umurcabuk ,
In order to download it, or get it in the search list, you need to have an active license.
BR
LFGP
Dear @LFGP
It automatically converts "QVCS 4.5" to "QVCS 4_5" after pressing search button and I've still cannot see the QCVS in Product Search even i searched as "QVCS 4.5". Could you please share it via Google Drive or etc...
Thank you!
dear @umurcabuk ,
please type QCVS 4.5 instead of 4_5, see the next
BR
LFGP
Dear @LFGP
I followed the steps you mentioned, but I still can't see QCVS. Is there another problem?
Thank you for your response!
Dear @umurcabuk ,
please follow the steps showed in the attached file.
Once in the last step, please type as next