2315088_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2315088_en-US

2315088_en-US

For S32G274A multi-core scenario, can the first 0x9100 bytes of fip.bin be neglected?
When making ATF image for BSP42, we get information like this:
Boot Core: A53_0
IVT Location: QSPI
Load address: 0x342f8f00
Entry point: 0x34302000
 
Entry point - Load address = 0x9100
it's BL2 that sits at offset 0x9100 of fip.bin. So is "Entry point" refering to BL2?
 
For multi-core scenario, MCU runs bootloader to load BL2 for A53.
If BL2 is the entry point, should bootloader just copy from offset 0x9100 of fip.bin(BL2) to 0x34302000 of RAM space(neglect the first 0x9100 bytes)?
GoldVIPRe: For S32G274A multi-core scenario, can the first 0x9100 bytes of fip.bin be neglected?

Hello, @wansp 

Thanks for your post

The bootloader will move the data from QSPI to the Load address(SRAM), they would not be neglected.


BR

Chenyin

Tags (1)
No ratings
Version history
Last update:
‎02-11-2026 05:23 AM
Updated by: