2314893_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2314893_en-US

2314893_en-US

FRDM-IMXRT1186

I want to use FRDM-IMXRT1186.

Application 1 > Board Should work with Internal 1.5MB RAM and with External QSPI Flash.

A> Ethernet 1 MII port (Named with Label ECAT0) can be configured with TCP/IP MODBUS Master ? 

B> Ethernet 2 MII port (Named with Label ECAT1) can be configured with ETHERCAT Master ?


Application 2 > Board Should work with Internal 1.5MB RAM and with External QSPI Flash. Arduino & MC Interface connector.

A> Ethernet 1 MII port (Named with Label ECAT0) & Ethernet 2 MII port (Named with Label ECAT1) can be used for Ethercat Slave & Arduino & MC Interface connector Analog/Digital GPIO ?

Re: FRDM-IMXRT1186

Hi @sarikaautomations ,

Thanks for your interest in NXP MIMXRT series!

1. A: It's recommend using J56A/J56B (RGMII ports for ETH0/ETH2) for TCP/IP/Modbus communication. Using J57A (ECAT0 port) is not advised.

B: No. The RT1180 integrates ESC, not an ECAT master.

2. Yes, this is supported.

For more detailed information, please refer to this guide: UM12450: FRDM-IMXRT1186 Board User Manual

Best regards,
Gavin

标记 (1)
无评分
版本历史
最后更新:
‎02-26-2026 02:42 AM
更新人: