I’m working with the RT700 evaluation board (MIMXRT700-EVK), and I’ve come across a discrepancy in the documentation. The block diagram mentions a Macronix flash memory part number as MX25UM51345GXDI00 , but this does not match the BOM file where it mentions MX25UW51345GXDI00. Additionally, the part number on the physical board itself differs from the block diagram
WhatsApp Image 2026-02-09 at 16.15.15 (2).jpeg
WhatsApp Image 2026-02-09 at 16.15.14 (1).jpeg
. This is causing confusion, especially when trying to reference documentation or locate the correct data sheet. Could you clarify the exact flash part number currently used on the RT700-EVK? Also, if possible, could NXP provide the data sheet for this specific flash IC? That would be extremely helpful for our development.
I only wanted to report this issue so that in the next errata or next revision of the RT700 EVK board manual NXP can take this into consideration. for the datasheet I'll contact macronix.
Hi @prathamvora,
Please follow the BOM for the memory part number. For the datasheet, please contact Macronix.
Best Regards,
Pablo
Hi,
Thank you for bringing this to our attention.
For future reference, you can also use the following link to submit technical documentation feedback.
Technical Documentation Feedback | NXP Semiconductors
Best Regards,
Pablo