2311174_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2311174_en-US

2311174_en-US

FRDM-MCXN947 Ethernet Issue

Hi NXP Community,

I just purchased 3 FRDM-MCXN947 dev kits for a company project and I can't get the Ethernet port to pass data on one of them.  I am using Zephyr v4.3.0 and I have tested using the `http_server` sample.  This works on the other two but I can't get DHCP or static IPs to work on the remaining on.  The link lights are lit but it just times out trying to get a DHCP address and when static it's not routable.  The device also doesn't show up as a client in our network management tools.

Thoughts on other tests I can run?  Has this happened before?

Thanks in advance,

Daz

Communication & Control(I3C | I2C | SPI | FlexCAN | Ethernet | FlexIO)Development BoardMCXNRe: FRDM-MCXN947 Ethernet Issue

Hi @WestCoastDaz 

May I ask if all three chips are the same? Has the board been reworked?

I think you can also test the SDK lwIP demos.

Harry_Zhang_0-1770257886923.png

If lwIP also fails to get DHCP or cannot respond to ping, I think this may be a hardware issue.

BR

Harry

Re: FRDM-MCXN947 Ethernet IssueUnfortunately I can't compare the chip versions as 2 of the DKs are being used in prototypes and I don't have access to them. The box on the non-working DK has a date code from 2429.

I don't have MCUXsspresso SDK installed only Zephyr is there another Zephyr example I could try?

Thanks,
Re: FRDM-MCXN947 Ethernet Issue

Hi @WestCoastDaz 

If you don't have MCUXsspresso SDK installed.

I think you can try to test the

samples/net/sockets/echo_server/

or

samples/net/dhcpv4_client

BR

Harry

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-10-2026 02:26 AM
更新者: