2304891_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2304891_en-US

2304891_en-US

I.MX9596 M7 core how to manually or automatically load in uboot phase

Hello.

At present, we are developing I.MX9596 chip, and have built the development environment of MCUXPresson for VSCode, which can compile M7 core normally. But how to load M7 core in uboot phase?

HL_G_0-1770084368819.png

We get a method, but we don't know how to implement it: To load M7 images in the Uboot phase, you need to compile System manager(M33) with imx95evkrpmsg. Copy your generated M7 image to the Boot (FAT32) partition of SD/eMMC. You can use this command in the Uboot phase.

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @Zhiming_Liu

We don't have the source code of FRDM to compile, can you provide the compiled image from your side, I will test it on the board.

Thank you!

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Tried both EVK and my own boards, same phenomenon, and since we don't have the source code for the EVK boards, we are using the mirrors you provided. Is it related to this
EVK:

HL_G_1-1770192493979.png

HL_G_0-1770192393151.png

Can you send me the M33 image from your side for testing?

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G
I'm using the imx-boot-variant-rpmsg-imx95-19x19-lpddr5-evk-sd.bin-flash_lpboot_sm_a55 inside the L6.12.49 demo image, and it's loadable. Are you currently using an EVK or a board you made yourself? If EVK, what is the exact model number?

Zhiming_Liu_0-1770191556077.png



Best Regards,
Zhiming

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @Zhiming_Liu

That's what's being used.

HL_G_0-1770191104231.png

mkimg compile command make SOC=iMX95 flash_a55 LPDDR_TYPE=lpddr4x OEI=YES

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

In addition to imx-sm using mx95evkrpmsg, flash_lpboot_sm_a55 is required for imx-mkimage .

Re: I.MX9596 M7 core how to manually or automatically load in uboot phaseHi.
We didn't build the yocto environment, we compiled it manually using imx-sm, imx-mkimage.
IMXBOOT_VARIANT= "rpmsg "What changes are made in the source code behind the options corresponding to these two.
Thanks!
Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Just compile imx-boot separately, with bitbake imx-boot, it's fast.

Re: I.MX9596 M7 core how to manually or automatically load in uboot phaseDoes this require a recompile of yocto? It will take a couple days to recompile.Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G

You add IMXBOOT_VARIANT= "rpmsg " to yocto's local.conf and try it with the following imx-boot.

Zhiming_Liu_0-1770187643964.png


Best Regards,
Zhiming

Re: I.MX9596 M7 core how to manually or automatically load in uboot phaseYes, same error loading the bin file.
Best Regards,
HL_G
Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G

Is it the same error loading the .bin

Best Regards,
Zhiming

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

In imx-sm there is the imx95evkrpmsg related configuration.

HL_G_0-1770103029093.png

Currently compiled the M33 core program according to this, and do not let the M33 start M7, the M7 bin file and elf file to the SD/eMMC Boot (FAT32) partition, the back is loaded in the uboot stage, the execution of the second step of the reboot error.

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @Zhiming_Liu 

An error occurs when loading the M7 core, as shown below:

HL_G_0-1770101121343.png

After the error, core A restarted, and M7 did not print information.


Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G
Specific steps in uboot:

Zhiming_Liu_1-1770097386025.png


To compile the M7 image into imx-boot for power-on booting, refer to the imx-mkimage section of the documentation

https://www.nxp.com/docs/en/user-guide/UG10163.pdf


Zhiming_Liu_0-1770097173224.png

There is no imx95evkrpmsg related configuration in imx-sm though .

https://github.com/nxp-imx/imx-sm/tree/master



Best Regards,
Zhiming

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G

This board and the corresponding yocto are still in beta, no official release, I can't test it at the moment. This rpmsg variant corresponds to mx95evkrpmsg for imx-sm, and lpboot_sm_a55 for imx-mkimage. check again to see if these two .bin's are actually updated in.

https://github.com/nxp-imx/meta-imx/blob/walnascar-6.12.49-2.2.0/meta-imx-bsp/conf/machine/include/i...

Best Regards,
Zhiming

Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hello @Zhiming_Liu

Testing on our own board, imx-mkimg compiled make SOC=iMX95 LPDDR_TYPE=lpddr4x OEI=YES flash_lpboot_sm_a55 results in the following image:

HL_G_0-1770363465740.png

imx-mkimg compile make SOC=iMX95 LPDDR_TYPE=lpddr4x OEI=YES The result of flash_lpboot_sm_all is shown below:

HL_G_1-1770363490956.png

All other firmware is the same and it fails to load and reboot is just uboot rebooting itself, M33 is normal, suspect that uboot is accessing points that it is not allowed to access, is there any method or suggestion about this?

Thank you!


Re: I.MX9596 M7 core how to manually or automatically load in uboot phase

Hi @HL_G

fatload actually loads the firmware to the address 0x90000000, try another address like 0x90100000. also you look at the real value of the variable $loadaddr.

Best Regards,
Zhiming

Tags (1)
No ratings
Version history
Last update:
‎02-10-2026 03:28 AM
Updated by: