2303826_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2303826_en-US

2303826_en-US

FS26 Wake Up Issue on ISOSPI Wake

My customer has an issue with FS26 PMIC

  1. After enabling AFE LPCM successfully, FS26 PMIC enters LPOFF mode with wake polarity configured as High.
  2. During an under‑voltage fault, the ISOSPI asserts the INTR pin from Low to High.
  3. This INTR signal is connected in parallel to FS26 WAKE1 and S32K322 GPIO PTC12.
  4. However, when INTR transitions to High, the line only reaches around 600 mV, which is not sufficient for FS26 to exit LPOFF. Due to this, FS26 is not waking up.

I would suspect loading on the shared WAKE/INTR net (e.g., MCU pin not fully Hi‑Z or weak/OD INTR driver), but I would appreciate if any guidance or recommendation to fix issue.


FS26 S32K3

Re: FS26 Wake Up Issue on ISOSPI Wake

Hi Allan (@AllanAn),

Could you please help with this question from our colleague Yuko-san?

Thanks & BRs, Tomas

Re: FS26 Wake Up Issue on ISOSPI Wake

Hi Yuko,

From your description, INTR too low leading to not reach FS26 WAKE pin high threshold, as a result, device did not wakeup.

I only suggest customer to have a high INTR voltage and I did not see any action from FS26 side, as it is customer responsibility to make sure wakeup signal should be valid within FS26 spec as attached.


Brs

Allan 

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎04-08-2026 03:40 AM
更新者: