2300889_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2300889_en-US

2300889_en-US

(88w8897) is disabling 2.4GHz capabilities possible?

Dear NXP,

Is it possible to switch off the 2.4GHz completely?
We want to disable the support for the 2.4GHz at the driver level.

From this link: Disable 5GHz band for 88W8987, we can see that during driver load, the dev_cap_mask can be used to enable support for specific bands. However, there is no documentation that explains how each bit of dev_cap_mask should be configured.

If we only want to switch off the 2.4GHz, what value should dev_cap_mask be set to?

Re: (88w8897) is disabling 2.4GHz capabilities possible?

Hi,


You can refer to https://community.nxp.com/t5/Wi-Fi-Bluetooth-802-15-4/How-to-disable-the-2-4GHz-band-on-the-88W8897/....


Regards,

Daniel.

Re: (88w8897) is disabling 2.4GHz capabilities possible?

Hi,

We would like to use dev_cap_mask to disable 2.4GHz capabilities.
Could you please provide us with more information about dev_cap_mask?

BR,
Peter

Tags (1)
No ratings
Version history
Last update:
‎02-03-2026 02:32 AM
Updated by: