Hello
I would like to confirm whether the OV5640 camera sensor is officially supported on the i.MX93 FRDM board.
I noticed that a device tree overlay named imx93-11x11-frdm-ov5640.dtso exists. However, I would like to know whether this support is fully validated and guaranteed for the i.MX93 FRDM board, or if it is provided for reference purposes only.
Could you please confirm if the OV5640 camera can be reliably used on the i.MX93 FRDM board and whether there are any required hardware connections or specific BSP versions that should be used.
Thank you
Hi @MinhVu
Yes, OV5640 can reliably used on the i.MX93 FRDM board. And you need to use our lf_6.12_x BSP code version. We have already verified it.
B.R
Do you have the driver and software setup instructions to run the OV5640 camera on the i.MX93 FRDM board?
Yes, the OV5640 is officially supported and verified on the i.MX93 FRDM board. The imx93-11x11-frdm-ov5640.dtso overlay is valid, not just a reference. Use the lf_6.12_x BSP and make sure the MIPI‑CSI, I²C, power