2296876_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2296876_en-US

2296876_en-US

RT1021 input max current

Hello, do you know how much current a GPIO input can handle? I'm using GPIO_AD_B1_02 and 8mA are flowing through that pin.

What is the maximum current an input can handle before damaging the pin?

The pin is on it's default values, if I understood right it is configured as input with 100k pulldown resistor by default

Thank you

Re: RT1021 input max current

Hi @jtrujillo,

In general, the maximum current for any RT1xxx GPIO pin should be limited to 25mA whether it is sourcing or sinking current. This is the safe limit for the technology to prevent reliability issues, like latent damage due to electromigration, and can be sustained for long durations if the pin needs to.

BR,
Edwin.

Tags (1)
No ratings
Version history
Last update:
‎01-22-2026 04:26 AM
Updated by: