2296668_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2296668_en-US

2296668_en-US

Power supply issue with FS32K142

Dear NXP experts

The MCU used in this design is FS32K142HFT0MLF.
My question is: can this device be powered with a 3.3 V supply, i.e., VDD = +3.3V ?

Looking forward to your reply.

best regard.

Far

Re: Power supply issue with FS32K142

Hi @Julián_AragónM 

I am glad to receive your reply.

Your answer has answered my question. Thank you very much.

Best regards

Far

Re: Power supply issue with FS32K142

Hi @FAR1234,

Yes. S32K1 can operate at 3.3V. It supports an operating supply voltage range from 2.7 V to 5.5 V. This means it can run on either 3.3 V or 5 V, depending on your design requirements.

You can refer to chapter 5.3 from S32K1xx Data Sheet for 5.3 DC electrical specifications at 3.3 V.

Best regards,
Julián

Tags (1)
No ratings
Version history
Last update:
‎01-21-2026 04:30 AM
Updated by: