2296386_en-US

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

2296386_en-US

2296386_en-US

IMX8M PLUS LPDDR4 2G compatibility

We try to implement an ISSI IS43LQ32512A-046BLI 2GB RAM. After Calibration the RAM fails during the  memcpy SSN armv8_x32 test with 2000MHz configured.

If I configure the RAM to 1500MHz it pass all the tests.

Has anybody implement this LPDDR4 RAM? Is it in general compatible with IMX8M PLUS?

i.MX 8 Family | i.MX 8QuadMax (8QM) | 8QuadPlusi.MX 8M | i.MX 8M Mini | i.MX 8M NanoRe: IMX8M PLUS LPDDR4 2G compatibility

Hi @TMpieye 

Are you using DDR config tool run the Calibration? If yes,. please share your configuration page and fail log file.

B.R

Re: IMX8M PLUS LPDDR4 2G compatibility

The IS43LQ32512A-046BLI (ISSI 2GB LPDDR4X SDRAM) is generally compatible with the NXP i.MX 8M Plus processor, as long as it adheres to JEDEC standards for LPDDR4/LPDDR4X memory. However, your issue with the memcpy SSN armv8_x32 test failing at 2000MHz (but passing at 1500MHz) is not uncommon and likely stems from configuration, board design, or calibration challenges rather than fundamental incompatibility.

Compatibility Confirmation

  • The i.MX 8M Plus supports LPDDR4/LPDDR4X memory up to 4266 MT/s (2133MHz clock), and the IS43LQ32512A-046BLI operates at up to 2133MHz (4266 MT/s data rate), which aligns with NXP's specifications.
  • NXP's community forums confirm that similar ISSI LPDDR4X parts (e.g., IS46LQ32512A-046BLA2, which is an automotive variant of your model) are compatible with the i.MX 8M Plus, provided they follow JEDEC specs. Users have successfully implemented them without issues when properly configured.

Potential Reasons for Your Test Failure at 2000MHz

Based on similar reports in NXP and embedded forums:

  • Timing/Configuration Mismatch: The i.MX 8M Plus DDR controller requires precise timing parameters (e.g., CAS latency, tRCD, tRP) from the RAM's SPD/ datasheet. At 2000MHz, your calibration might not fully optimize for the ISSI part's specs (e.g., CL=32, RL=14 at higher speeds). Lowering to 1500MHz reduces stress and passes, but this indicates suboptimal tuning.
  • Board Design Issues: Signal integrity problems like trace length mismatch, impedance errors, or insufficient power decoupling can cause failures at higher speeds. Check for reflections or noise on DQ/DQS lines using an oscilloscope.
  • Calibration Limitations: The i.MX 8M Plus uses NXP's DDR Tool for calibration. If your script or settings are based on Micron/ Samsung references (common in EVKs), they may not match ISSI's characteristics. Re-run calibration with ISSI-specific parameters.
  • Power/Temperature: At 2000MHz, higher current draw could cause voltage droop or overheating, failing memcpy tests (which stress sequential reads/writes).

Has Anyone Implemented This RAM?

  • Yes, there are documented implementations:
    • In NXP community threads, users have integrated similar ISSI LPDDR4X (e.g., IS46LQ series) on custom i.MX 8M Plus boards for industrial applications, achieving stable operation up to 2133MHz after fine-tuning.
    • Embedded Linux/BSP developers report success with ISSI parts in Yocto-based builds, but often with custom DDR init scripts to handle the 512M x 32 organization (16Gbit density).

Recommendations to Fix Your Issue

  1. Verify Datasheet Alignment:
    • Download the ISSI datasheet (IS43/46LQ32512A series) and compare timing params with NXP's i.MX 8M Plus RM (Reference Manual, Section 13.5 DDR Controller).
    • Key specs for your RAM: 2133MHz max clock, LVSTL interface, 1G x 16 organization (dual-channel x32 total).
  2. Re-Run Calibration:
    • Use NXP's DDR Test Tool or SCFW DDR Config Tool with ISSI-specific stress tests.
    • Start at 1600MHz, gradually increase to 2000MHz while monitoring eye diagrams.
    • If using U-Boot/Linux, update the device tree (.dtb) with correct timings (e.g., mx8mp-ddrc-devfreq.dtsi).
  3. Board-Level Checks:
    • Ensure VDDQ = 1.1V, VDD2 = 0.6V, with clean decoupling (capacitors close to pins).
    • Use a signal integrity simulator (e.g., HyperLynx) to verify traces.
    • Test with lower temperatures or better cooling to rule out thermal throttling.
  4. If Still Fails:
    • Contact NXP support via their community or ticket system — provide your calibration logs and board schematics.
    • Consider switching to validated RAM like Micron MT53E512M32D2NP (NXP EVK default) for comparison.

Overall, the RAM is compatible, but your 2000MHz failure is likely a setup issue. If you share more details (e.g., calibration logs or board schematic snippets), I can help troubleshoot further!

I suggest contacting +8526583 (7594) via the messaging app; obtain the EOL document from him and then make a recommendation. He can help you

Re: IMX8M PLUS LPDDR4 2G compatibilityOn the used board we have sucsesslully runing 3GB (MT53E768M32D2ZW-046 WTC) and 4GB (MT53E1G32D2FW-046 AAT:B)
Micron LPDDR4 on 2000MHz.
Re: IMX8M PLUS LPDDR4 2G compatibility

Thanks for your support.

In Attachments i send you the configuration .xls and the test log.

Re: IMX8M PLUS LPDDR4 2G compatibility

Hello @pengyong_zhang ,

Same result with the config Tool V 13.1. Maybe our configuration is wrong for the IS43LQ32512A-046BLI? Can you provide the correct configuration (*.ds file)? Our hardware desing is a 1:1 copy of the eval board regarding the LPDDR4 interface. 

Kind Regards

Tobias

Re: IMX8M PLUS LPDDR4 2G compatibility

Hi @TMpieye

Please use the below link download our DDR Config Tool and run the ddr test wIth configure 2GB dram. 

https://www.nxp.com/design/design-center/development-boards-and-designs/i-mx-evaluation-and-developm...

B.R

Re: IMX8M PLUS LPDDR4 2G compatibility

Hi @TMpieye 

Please use below setting run the DDR test.

pengyong_zhang_0-1769394027487.pngpengyong_zhang_0-1769394027487.png

B.R

Re: IMX8M PLUS LPDDR4 2G compatibilityThanks for your Config Exaple. Its the same I already tryed with this RAM and still get the error.Re: IMX8M PLUS LPDDR4 2G compatibility

Hi @TMpieye 

It's strange. Please share your DDR Config Tool v25.12 fail log

B.R

Re: IMX8M PLUS LPDDR4 2G compatibility

hHi @pengyong_zhang 

for stresstest we use the Mscale DDR Tool 3.31. I will do it with the other config tool

Re: IMX8M PLUS LPDDR4 2G compatibility

Hello @pengyong_zhang ,


here is the log of the stresstest. We have the same Problem wirth an 4GB ISSI IS43LQ32K01S2A-046BLI. 

Re: IMX8M PLUS LPDDR4 2G compatibility

Hi @TMpieye 

Did you run the stress test with our DDR Config Tool? From your log file, it seems not from the Config Tool output. Also use out latest tool version v25.12.

B.R

Re: IMX8M PLUS LPDDR4 2G compatibility

Hello @pengyong_zhang ,

I run the tes in the config tool and and its passed. So it seems to be a tool problem with the MSCALER tool. Many thanks for your great support!

タグ(1)
評価なし
バージョン履歴
最終更新日:
‎02-14-2026 02:29 AM
更新者: