2295732_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2295732_en-US

2295732_en-US

imx8ulp-evk: Yocto 5.2 (L6.12.49) build failure with tensorflow-lite-vx-delegate / litert-vx-delegat

Hello,

I am building imx-image-full for i.MX8ULP EVK using NXP Yocto 5.2 (kernel L6.12.49) and encounter build failures related to tensorflow-lite-vx-delegate and litert-vx-delegate.

Both packages fail during the download/verify step when fetching kleidiai from Arm GitLab, resulting in a SHA256 checksum mismatch.

The issue is reproducible for:

tensorflow-lite-vx-delegate (2.19.0)

litert-vx-delegate (1.2.0)

It appears that the upstream kleidiai archive content has changed while keeping the same commit hash, causing the checksum defined in the recipes to be invalid.

Full build logs for both packages are attached below.

Questions:

Is this a known issue in Yocto 5.2?

Is there an official fix or updated checksum?

Thanks in advance.

i.MX8ULPYocto ProjectRe: imx8ulp-evk: Yocto 5.2 (L6.12.49) build failure with tensorflow-lite-vx-delegate / litert-vx-del

$ bitbake tensorflow-lite-vx-delegate -c cleansstate

$ bitbake tensorflow-lite-vx-delegate -c patch

$ cd build/tmp/work/armv8a-poky-linux/tensorflow-lite-vx-delegate/2.19.0/sources-unpack/tfgit

$ patch -p1 <0001-Fix-source-sha256-mismatch-issue-for-KleidiAI.patch

$ bitbake tensorflow-lite-vx-delegate

Re: imx8ulp-evk: Yocto 5.2 (L6.12.49) build failure with tensorflow-lite-vx-delegate / litert-vx-del

I ran into the same tensorflow-lite build failure related to kleidiai on Yocto for the frdm-imx93 board. Here is my solution:
cd sources/meta-imx
patch -Np1 -i 0001-Fixed-KleidiAI-sha256-mismatch.patch
This solution does not patch tensorflow itself. I think this is a clearer solution.

Re: imx8ulp-evk: Yocto 5.2 (L6.12.49) build failure with tensorflow-lite-vx-delegate / litert-vx-del

Thank you for the suggestion.

Instead of modifying the downloaded source directly, I applied the workaround properly via a custom meta layer.

After applying this change, the build issue of tensorflow-lite-vx-delegate is resolved successfully.


However, litert-vx-delegate still fails with the same kleidiai SHA256 checksum mismatch during the download step.

Do you have any suggestion for litert-vx-delegate, or is there a separate fix planned for this package?

Re: imx8ulp-evk: Yocto 5.2 (L6.12.49) build failure with tensorflow-lite-vx-delegate / litert-vx-del

Please refer to the attached patch.

Tags (1)
No ratings
Version history
Last update:
‎01-30-2026 02:23 AM
Updated by: