2295523_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2295523_en-US

2295523_en-US

iMX RT700 EVK accessing SDIO Card

Trying to access 1.8V SDIO card on RT700 EVK. Set jumpers JP65 and JP66 to 1-2 using a sample enhanced with debug statements.

SDCARD fatfs freertos example.

Card inserted.

SDCARD fatfs freertos example.

Card inserted.

--- SD Card Init ---
SD card init failed! Status: 1834
Possible causes:
- Card doesn't support 1.8V signaling
- Voltage switch failed
- Card communication error

Trying basic card detection...
OCR: 0x 0
Flags: 0x 0

Re: iMX RT700 EVK accessing SDIO Card

Hi @MikeAtPhantom ,

Thank you so much for your interest in our products and for using our community.

Please carefully check the readme file.

I did a test for you, the SDK demo runs okay.

HW: MIMXRT700-EVK    JP65 1-2 connected

SW:  mimxrt700evk_sdcard_fatfs_freertos_cm33_core0

SD:    SanDisk  Ultra   32G

mayliu1_0-1768795490345.png

Please use Recommend SD Cards , and try to run the example again.

Best Regards

MayLiu

Tags (1)
No ratings
Version history
Last update:
‎01-20-2026 04:24 AM
Updated by: