2295454_en-US

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

2295454_en-US

2295454_en-US

Expected v30 U3 SD CARD Write Performance on MIMXRT1020-EVK

Starting with the sdcard_fatfs example in MCUXpresso, and adding the semc driver, I am able to declare an array in SDRAM and write large amounts of data from SDRAM to the SDCARD. Using a SanDisk V30 U3 card, I get 20MB written in 2119ms and 3MB written in 311ms. Is this result within the expected performance? Are there particular parameters I can tune for V30 U3 to improve it?


Thanks,

Doug

Re: Expected v30 U3 SD CARD Write Performance on MIMXRT1020-EVK

Hi @dougcl ,

Thank you so much for your interest in our products and for using our community.

Regarding your question, the entire time include reading data from Sdram, and write to SD card? I think the  result within the expected performance.

For SDRAM high performance, I suggest you can refer to this AN  

AN12437: i.MX RT Series Performance Optimization – Application Note

For USDHC, I suggest you use the 4 bit mode in stead of 1 bit mode(if you use uSDHC1), and also use DMA to transfer data.

mayliu1_0-1768890285160.pngmayliu1_0-1768890285160.png

You can also refer to the AN below.

 Using the i.MXRT L1 Cache

Best Regards

MayLiu

标记 (1)
无评分
版本历史
最后更新:
‎01-21-2026 04:32 AM
更新人: