2292973_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2292973_en-US

2292973_en-US

Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6

We've got Voipac iMX6 Rex UltraPlus dev kit. It comes with linux 4.1. I wanted to get mordern linux so I got linux-imx branch lf-6.6.y and imx_v7_defconfig. I tried porting the device tree and 

// SPDX-License-Identifier: GPL-2.0-only
/*
 * Copyright 2014 FEDEVEL, Inc.
 *
 * Author: Robert Nelson 
 */
/dts-v1/;
#include "imx6q.dtsi"
#include "imx6qp.dtsi"
#include "imx6qdl-rex.dtsi"

/ {
	model = "Rex Pro i.MX6 Quad Board";
	compatible = "rex,imx6q-rex-pro", "fsl,imx6q";

	memory: memory@10000000 {
		device_type = "memory";
		reg = <0x10000000 0x80000000>;
	};
};

&ecspi3 {
	flash: flash@0 {
		compatible = "sst,sst25vf032b", "jedec,spi-nor";
		spi-max-frequency = <20000000>;
		reg = <0>;
	};
};


&i2c2 {
	clock-frequency = <100000>;
	pinctrl-names = "default";
	pinctrl-0 = <&pinctrl_i2c2>;
	status = "okay";

	hdmi_ddc: edid@50 {
		compatible = "fsl,imx6-hdmi-i2c";
		reg = <0x50>;
	};

};

&sata {
	status = "okay";
};

&mxcfb1 {
	prefetch;
	status = "okay";
};

&mxcfb2 {
	prefetch;
	status = "okay";
};

&mxcfb3 {
	prefetch;
	status = "disabled";
};

&mxcfb4 {
	prefetch;
	status = "disabled";
};

&pre1 {
	status = "okay";
};

&pre2 {
	status = "okay";
};

&pre3 {
	status = "okay";
};

&pre4 {
	status = "okay";
};

&prg1 {
	memory-region = <&memory>;
	status = "okay";
};

&prg2 {
	memory-region = <&memory>;
	status = "okay";
};

&hdmi_core {
	ipu_id = <0>;
	disp_id = <0>;
	status = "okay";
};

&hdmi_video {
	fsl,phy_reg_vlev = <0x0294>;
	fsl,phy_reg_cksymtx = <0x800d>;
	status = "okay";
};

There seems to be a problem in PRE -> PRG -> IPU -> HDMI pipeline. 

Starting kernel ...

[    0.000000] Booting Linux on physical CPU 0x0
[    0.000000] Linux version 6.6.52-g5a0a5e71d2bd-dirty (anurag@anurag-SK5800) (arm-linux-gnueabi-gcc (Ubuntu 13.3.0-6ubuntu2~24.04) 13.3.0, GNU ld (GNU Binutils for Ubuntu) 2.42) #29 SMP PREEMPT Tue Jan 13 15:33:15 IST 2026
[    0.000000] CPU: ARMv7 Processor [412fc09a] revision 10 (ARMv7), cr=10c5387d
[    0.000000] CPU: PIPT / VIPT nonaliasing data cache, VIPT aliasing instruction cache
[    0.000000] OF: fdt: Machine model: Rex Pro i.MX6 Quad Board
[    0.000000] Memory policy: Data cache writealloc
[    0.000000] Reserved memory: created CMA memory pool at 0xea000000, size 320 MiB
[    0.000000] OF: reserved mem: initialized node linux,cma, compatible id shared-dma-pool
[    0.000000] OF: reserved mem: 0xea000000..0xfdffffff (327680 KiB) map reusable linux,cma
[    0.000000] Zone ranges:
[    0.000000]   Normal   [mem 0x0000000010000000-0x000000007fffffff]
[    0.000000]   HighMem  [mem 0x0000000080000000-0x00000000ffffefff]
[    0.000000] Movable zone start for each node
[    0.000000] Early memory node ranges
[    0.000000]   node   0: [mem 0x0000000010000000-0x00000000ffffefff]
[    0.000000] Initmem setup node 0 [mem 0x0000000010000000-0x00000000ffffefff]
[    0.000000] percpu: Embedded 12 pages/cpu s18900 r8192 d22060 u49152
[    0.000000] Kernel command line: console=ttymxc0,115200 root=/dev/nfs nfsroot=192.168.1.41:/srv/nfsroot,v3 rw ip=dhcp
[    0.000000] Dentry cache hash table entries: 262144 (order: 8, 1048576 bytes, linear)
[    0.000000] Inode-cache hash table entries: 131072 (order: 7, 524288 bytes, linear)
[    0.000000] Built 1 zonelists, mobility grouping on.  Total pages: 979007
[    0.000000] mem auto-init: stack:all(zero), heap alloc:off, heap free:off
[    0.000000] Memory: 3544512K/3932156K available (14336K kernel code, 1522K rwdata, 4944K rodata, 1024K init, 425K bss, 59964K reserved, 327680K cma-reserved, 1769468K highmem)
[    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=4, Nodes=1
[    0.000000] rcu: Preemptible hierarchical RCU implementation.
[    0.000000] rcu: 	RCU event tracing is enabled.
[    0.000000] 	Trampoline variant of Tasks RCU enabled.
[    0.000000] rcu: RCU calculated value of scheduler-enlistment delay is 10 jiffies.
[    0.000000] NR_IRQS: 16, nr_irqs: 16, preallocated irqs: 16
[    0.000000] L2C: DT/platform modifies aux control register: 0x32070000 -> 0x32470000
[    0.000000] L2C-310 erratum 769419 enabled
[    0.000000] L2C-310 enabling early BRESP for Cortex-A9
[    0.000000] L2C-310 full line of zeros enabled for Cortex-A9
[    0.000000] L2C-310 ID prefetch enabled, offset 16 lines
[    0.000000] L2C-310 dynamic clock gating enabled, standby mode enabled
[    0.000000] L2C-310 cache controller enabled, 16 ways, 1024 kB
[    0.000000] L2C-310: CACHE_ID 0x410000c8, AUX_CTRL 0x76470001
[    0.000000] rcu: srcu_init: Setting srcu_struct sizes based on contention.
[    0.000000] Switching to timer-based delay loop, resolution 333ns
[    0.000001] sched_clock: 32 bits at 3000kHz, resolution 333ns, wraps every 715827882841ns
[    0.000026] clocksource: mxc_timer1: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 637086815595 ns
[    0.001453] Console: colour dummy device 80x30
[    0.001498] Calibrating delay loop (skipped), value calculated using timer frequency.. 6.00 BogoMIPS (lpj=30000)
[    0.001518] CPU: Testing write buffer coherency: ok
[    0.001562] CPU0: Spectre v2: using BPIALL workaround
[    0.001573] pid_max: default: 32768 minimum: 301
[    0.001769] Mount-cache hash table entries: 4096 (order: 2, 16384 bytes, linear)
[    0.001804] Mountpoint-cache hash table entries: 4096 (order: 2, 16384 bytes, linear)
[    0.002831] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
[    0.004268] RCU Tasks: Setting shift to 2 and lim to 1 rcu_task_cb_adjust=1.
[    0.004454] Setting up static identity map for 0x10100000 - 0x10100060
[    0.004688] rcu: Hierarchical SRCU implementation.
[    0.004694] rcu: 	Max phase no-delay instances is 1000.
[    0.006556] smp: Bringing up secondary CPUs ...
[    0.007512] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
[    0.007532] CPU1: Spectre v2: using BPIALL workaround
[    0.008616] CPU2: thread -1, cpu 2, socket 0, mpidr 80000002
[    0.008634] CPU2: Spectre v2: using BPIALL workaround
[    0.009701] CPU3: thread -1, cpu 3, socket 0, mpidr 80000003
[    0.009720] CPU3: Spectre v2: using BPIALL workaround
[    0.009851] smp: Brought up 1 node, 4 CPUs
[    0.009868] SMP: Total of 4 processors activated (24.00 BogoMIPS).
[    0.009878] CPU: All CPU(s) started in SVC mode.
[    0.011183] devtmpfs: initialized
[    0.020354] VFP support v0.3: implementor 41 architecture 3 part 30 variant 9 rev 4
[    0.020648] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
[    0.020675] futex hash table entries: 1024 (order: 4, 65536 bytes, linear)
[    0.038260] pinctrl core: initialized pinctrl subsystem
[    0.039950] NET: Registered PF_NETLINK/PF_ROUTE protocol family
[    0.047487] DMA: preallocated 256 KiB pool for atomic coherent allocations
[    0.048756] thermal_sys: Registered thermal governor 'step_wise'
[    0.048832] cpuidle: using governor menu
[    0.049055] CPU identified as i.MX6QP, silicon rev 1.0
[    0.057573] platform soc: Fixed dependency cycle(s) with /soc/bus@2000000/gpc@20dc000
[    0.058532] platform 120000.hdmi: Fixed dependency cycle(s) with /soc/ipu@2800000
[    0.058565] platform 120000.hdmi: Fixed dependency cycle(s) with /soc/ipu@2400000
[    0.065172] mxs_phy 20c9000.usbphy: supply phy-3p0 not found, using dummy regulator
[    0.065766] mxs_phy 20ca000.usbphy: supply phy-3p0 not found, using dummy regulator
[    0.067266] platform 20dc000.gpc: Fixed dependency cycle(s) with /soc/bus@2000000/clock-controller@20c4000
[    0.069057] platform 20e0000.iomuxc-gpr:ipu1_csi0_mux: Fixed dependency cycle(s) with /soc/ipu@2400000
[    0.069276] platform 20e0000.iomuxc-gpr:ipu2_csi1_mux: Fixed dependency cycle(s) with /soc/ipu@2800000
[    0.069515] platform 20e0000.pinctrl: Fixed dependency cycle(s) with /soc/bus@2000000/pinctrl@20e0000/imx6qdl-rex/hoggrp
[    0.075192] platform 20e0000.iomuxc-gpr:ipu1_csi0_mux: Fixed dependency cycle(s) with /soc/ipu@2400000
[    0.075299] platform 120000.hdmi: Fixed dependency cycle(s) with /soc/ipu@2400000
[    0.075404] platform 2400000.ipu: Fixed dependency cycle(s) with /soc/hdmi@120000
[    0.075496] platform 2400000.ipu: Fixed dependency cycle(s) with /soc/bus@2000000/iomuxc-gpr@20e0000/ipu1_csi0_mux
[    0.076923] platform 20e0000.iomuxc-gpr:ipu2_csi1_mux: Fixed dependency cycle(s) with /soc/ipu@2800000
[    0.077039] platform 120000.hdmi: Fixed dependency cycle(s) with /soc/ipu@2800000
[    0.077125] platform 2800000.ipu: Fixed dependency cycle(s) with /soc/hdmi@120000
[    0.077210] platform 2800000.ipu: Fixed dependency cycle(s) with /soc/bus@2000000/iomuxc-gpr@20e0000/ipu2_csi1_mux
[    0.080562] No ATAGs?
[    0.080724] hw-breakpoint: found 5 (+1 reserved) breakpoint and 1 watchpoint registers.
[    0.080738] hw-breakpoint: maximum watchpoint size is 4 bytes.
[    0.081653] imx6q-pinctrl 20e0000.pinctrl: initialized IMX pinctrl driver
[    0.085204] imx mu driver is registered.
[    0.085646] imx rpmsg driver is registered.
[    0.087876] kprobes: kprobe jump-optimization is enabled. All kprobes are optimized if possible.
[    0.089669] gpio gpiochip0: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.091854] gpio gpiochip1: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.093802] gpio gpiochip2: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.095768] gpio gpiochip3: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.097730] gpio gpiochip4: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.099770] gpio gpiochip5: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.101758] gpio gpiochip6: Static allocation of GPIO base is deprecated, use dynamic allocation.
[    0.107751] SCSI subsystem initialized
[    0.108266] usbcore: registered new interface driver usbfs
[    0.108311] usbcore: registered new interface driver hub
[    0.108358] usbcore: registered new device driver usb
[    0.108509] usb_phy_generic usbphynop1: dummy supplies not allowed for exclusive requests
[    0.108714] usb_phy_generic usbphynop2: dummy supplies not allowed for exclusive requests
[    0.110687] i2c i2c-0: IMX I2C adapter registered
[    0.112084] pca953x 1-0027: using no AI
[    0.139188] pca953x 1-0027: interrupt support not compiled in
[    0.159914] i2c i2c-1: IMX I2C adapter registered
[    0.160673] i2c i2c-2: IMX I2C adapter registered
[    0.161268] mc: Linux media interface: v0.10
[    0.161343] videodev: Linux video capture interface: v2.00
[    0.161431] pps_core: LinuxPPS API ver. 1 registered
[    0.161438] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti 
[    0.161463] PTP clock support registered
[    0.162678] imx-ipuv3 2400000.ipu: 
[    0.162705] imx-ipuv3 2400000.ipu: revision is IPUv3H
[    0.163023] imx-ipuv3 2400000.ipu: IPU CM Regs = (ptrval)
[    0.163039] imx-ipuv3 2400000.ipu: IPU IC Regs = (ptrval)
[    0.163050] imx-ipuv3 2400000.ipu: IPU IDMAC Regs = (ptrval)
[    0.163057] imx-ipuv3 2400000.ipu: IPU DP Regs = (ptrval)
[    0.163065] imx-ipuv3 2400000.ipu: IPU DC Regs = (ptrval)
[    0.163072] imx-ipuv3 2400000.ipu: IPU DMFC Regs = (ptrval)
[    0.163080] imx-ipuv3 2400000.ipu: IPU DI0 Regs = (ptrval)
[    0.163087] imx-ipuv3 2400000.ipu: IPU DI1 Regs = (ptrval)
[    0.163095] imx-ipuv3 2400000.ipu: IPU SMFC Regs = (ptrval)
[    0.163102] imx-ipuv3 2400000.ipu: IPU CSI0 Regs = (ptrval)
[    0.163109] imx-ipuv3 2400000.ipu: IPU CSI1 Regs = (ptrval)
[    0.163117] imx-ipuv3 2400000.ipu: IPU CPMem = (ptrval)
[    0.163125] imx-ipuv3 2400000.ipu: IPU TPMem = (ptrval)
[    0.163133] imx-ipuv3 2400000.ipu: IPU DC Template Mem = (ptrval)
[    0.163141] imx-ipuv3 2400000.ipu: IPU VDI Regs = (ptrval)
[    0.163349] imx-ipuv3 2800000.ipu: 
[    0.163374] imx-ipuv3 2800000.ipu: revision is IPUv3H
[    0.163681] imx-ipuv3 2800000.ipu: IPU CM Regs = (ptrval)
[    0.163694] imx-ipuv3 2800000.ipu: IPU IC Regs = (ptrval)
[    0.163701] imx-ipuv3 2800000.ipu: IPU IDMAC Regs = (ptrval)
[    0.163709] imx-ipuv3 2800000.ipu: IPU DP Regs = (ptrval)
[    0.163716] imx-ipuv3 2800000.ipu: IPU DC Regs = (ptrval)
[    0.163723] imx-ipuv3 2800000.ipu: IPU DMFC Regs = (ptrval)
[    0.163729] imx-ipuv3 2800000.ipu: IPU DI0 Regs = (ptrval)
[    0.163736] imx-ipuv3 2800000.ipu: IPU DI1 Regs = (ptrval)
[    0.163743] imx-ipuv3 2800000.ipu: IPU SMFC Regs = (ptrval)
[    0.163750] imx-ipuv3 2800000.ipu: IPU CSI0 Regs = (ptrval)
[    0.163757] imx-ipuv3 2800000.ipu: IPU CSI1 Regs = (ptrval)
[    0.163763] imx-ipuv3 2800000.ipu: IPU CPMem = (ptrval)
[    0.163770] imx-ipuv3 2800000.ipu: IPU TPMem = (ptrval)
[    0.163778] imx-ipuv3 2800000.ipu: IPU DC Template Mem = (ptrval)
[    0.163785] imx-ipuv3 2800000.ipu: IPU VDI Regs = (ptrval)
[    0.164339] mxc_vdoa 21e4000.vdoa: iram_base:0xf0940000,iram_paddr:0x905000,size:0x12000
[    0.164358] mxc_vdoa 21e4000.vdoa: i.MX Video Data Order Adapter(VDOA) driver probed
[    0.164777] imx-prg 21cc000.prg: driver probed
[    0.164928] imx-prg 21cd000.prg: driver probed
[    0.165408] imx-pre 21c8000.pre: driver probed
[    0.165719] imx-pre 21c9000.pre: driver probed
[    0.166014] imx-pre 21ca000.pre: driver probed
[    0.166306] imx-pre 21cb000.pre: driver probed
[    0.166615] MIPI CSI2 driver module loaded
[    0.166665] Advanced Linux Sound Architecture Driver Initialized.
[    0.168110] Bluetooth: Core ver 2.22
[    0.168159] NET: Registered PF_BLUETOOTH protocol family
[    0.168167] Bluetooth: HCI device and connection manager initialized
[    0.168181] Bluetooth: HCI socket layer initialized
[    0.168191] Bluetooth: L2CAP socket layer initialized
[    0.168212] Bluetooth: SCO socket layer initialized
[    0.168645] vgaarb: loaded
[    0.169232] clocksource: Switched to clocksource mxc_timer1
[    0.169539] VFS: Disk quotas dquot_6.6.0
[    0.169596] VFS: Dquot-cache hash table entries: 1024 (order 0, 4096 bytes)
[    0.181120] NET: Registered PF_INET protocol family
[    0.181747] IP idents hash table entries: 32768 (order: 6, 262144 bytes, linear)
[    0.184933] tcp_listen_portaddr_hash hash table entries: 1024 (order: 1, 8192 bytes, linear)
[    0.184988] Table-perturb hash table entries: 65536 (order: 6, 262144 bytes, linear)
[    0.185067] TCP established hash table entries: 16384 (order: 4, 65536 bytes, linear)
[    0.185229] TCP bind hash table entries: 16384 (order: 6, 262144 bytes, linear)
[    0.185739] TCP: Hash tables configured (established 16384 bind 16384)
[    0.185938] UDP hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.186015] UDP-Lite hash table entries: 1024 (order: 3, 32768 bytes, linear)
[    0.186259] NET: Registered PF_UNIX/PF_LOCAL protocol family
[    0.186896] RPC: Registered named UNIX socket transport module.
[    0.186907] RPC: Registered udp transport module.
[    0.186913] RPC: Registered tcp transport module.
[    0.186917] RPC: Registered tcp-with-tls transport module.
[    0.186924] RPC: Registered tcp NFSv4.1 backchannel transport module.
[    0.188518] PCI: CLS 0 bytes, default 64
[    0.189143] armv7-pmu pmu: hw perfevents: no interrupt-affinity property, guessing.
[    0.189492] hw perfevents: enabled with armv7_cortex_a9 PMU driver, 7 counters available
[    0.192313] Bus freq driver module loaded
[    0.193564] Initialise system trusted keyrings
[    0.193855] workingset: timestamp_bits=14 max_order=20 bucket_order=6
[    0.194593] NFS: Registering the id_resolver key type
[    0.194649] Key type id_resolver registered
[    0.194657] Key type id_legacy registered
[    0.194693] nfs4filelayout_init: NFSv4 File Layout Driver Registering...
[    0.194703] nfs4flexfilelayout_init: NFSv4 Flexfile Layout Driver Registering...
[    0.194744] jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.
[    0.195069] fuse: init (API version 7.39)
[    0.335183] Key type asymmetric registered
[    0.335195] Asymmetric key parser 'x509' registered
[    0.335305] bounce: pool size: 64 pages
[    0.335338] io scheduler mq-deadline registered
[    0.335348] io scheduler kyber registered
[    0.335381] io scheduler bfq registered
[    0.341513] mxc_hdmi 20e0000.hdmi_video: hdcp disable
[    0.341791] mxc_hdmi 20e0000.hdmi_video: supply HDMI not found, using dummy regulator
[    0.342866] mxc_sdc_fb fb@0: mxcfb_probe enter
[    0.343005] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init
[    0.343023] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init - default mode 1920x1080M@60 bpp=24
[    0.343076] mxc_hdmi 20e0000.hdmi_video: Enabled HDMI clocks
[    0.343088] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[    0.343120] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[    0.343228] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init exit
[    0.343241] mxc_sdc_fb fb@0: di_pixfmt:0x33424752, bpp:0x18, di:0, ipu:0
[    0.343255] mxc_sdc_fb fb@0: registered mxc display driver hdmi
[    0.343266] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_deinit
[    0.343371] mxc_sdc_fb fb@1: mxcfb_probe enter
[    0.343388] mxc_sdc_fb fb@1: get of property mode_str fail
[    0.343405] mxc_sdc_fb fb@1: NO mxc display driver found!
[    0.347745] imx-sdma 20ec000.dma-controller: Direct firmware load for imx/sdma/sdma-imx6q.bin failed with error -2
[    0.347765] imx-sdma 20ec000.dma-controller: Falling back to sysfs fallback for: imx/sdma/sdma-imx6q.bin
[    0.349746] mxs-dma 110000.dma-controller: initialized
[    0.356074] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 283, base_baud = 5000000) is a IMX
[    0.356137] printk: console [ttymxc0] enabled
[    1.770772] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 284, base_baud = 5000000) is a IMX
[    1.780999] imx sema4 driver is registered.
[    1.800787] brd: module loaded
[    1.812434] loop: module loaded
[    1.815837] at24 1-0057: supply vcc not found, using dummy regulator
[    1.823438] at24 1-0057: 256 byte 24c02 EEPROM, writable, 1 bytes/write
[    1.832399] ahci-imx 2200000.sata: fsl,transmit-level-mV not specified, using 00000024
[    1.840381] ahci-imx 2200000.sata: fsl,transmit-boost-mdB not specified, using 00000480
[    1.848398] ahci-imx 2200000.sata: fsl,transmit-atten-16ths not specified, using 00002000
[    1.856610] ahci-imx 2200000.sata: fsl,receive-eq-mdB not specified, using 05000000
[    1.864374] ahci-imx 2200000.sata: supply ahci not found, using dummy regulator
[    1.871891] ahci-imx 2200000.sata: supply phy not found, using dummy regulator
[    1.879193] ahci-imx 2200000.sata: supply target not found, using dummy regulator
[    1.889925] ahci-imx 2200000.sata: SSS flag set, parallel bus scan disabled
[    1.896922] ahci-imx 2200000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
[    1.905794] ahci-imx 2200000.sata: flags: ncq sntf stag pm led clo only pmp pio slum part ccc apst 
[    1.916410] scsi host0: ahci-imx
[    1.919969] ata1: SATA max UDMA/133 mmio [mem 0x02200000-0x02203fff] port 0x100 irq 285
[    1.933418] spi-nor spi2.0: found sst26vf064b, expected sst25vf032b
[    1.939920] imx-sdma 20ec000.dma-controller: sdma or sdma firmware not ready!
[    1.948437] spi-nor spi2.0: sst26vf064b (8192 Kbytes)
[    1.958027] tun: Universal TUN/TAP device driver, 1.6
[    1.963393] CAN device driver interface
[    1.969204] e1000e: Intel(R) PRO/1000 Network Driver
[    1.974220] e1000e: Copyright(c) 1999 - 2015 Intel Corporation.
[    1.980653] usbcore: registered new device driver r8152-cfgselector
[    1.986967] usbcore: registered new interface driver r8152
[    1.992522] usbcore: registered new interface driver lan78xx
[    1.998221] usbcore: registered new interface driver asix
[    2.003694] usbcore: registered new interface driver ax88179_178a
[    2.009866] usbcore: registered new interface driver cdc_ether
[    2.015738] usbcore: registered new interface driver smsc95xx
[    2.021547] usbcore: registered new interface driver net1080
[    2.027245] usbcore: registered new interface driver cdc_subset
[    2.033233] usbcore: registered new interface driver zaurus
[    2.038845] usbcore: registered new interface driver MOSCHIP usb-ethernet driver
[    2.046328] usbcore: registered new interface driver cdc_ncm
[    2.052057] usbcore: registered new interface driver r8153_ecm
[    2.058033] usbcore: registered new interface driver usb-storage
[    2.066104] imx_usb 2184000.usb: No over current polarity defined
[    2.076502] ci_hdrc ci_hdrc.0: EHCI Host Controller
[    2.081461] ci_hdrc ci_hdrc.0: new USB bus registered, assigned bus number 1
[    2.109250] ci_hdrc ci_hdrc.0: USB 2.0 started, EHCI 1.00
[    2.114949] usb usb1: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.06
[    2.123265] usb usb1: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    2.130531] usb usb1: Product: EHCI Host Controller
[    2.135423] usb usb1: Manufacturer: Linux 6.6.52-g5a0a5e71d2bd-dirty ehci_hcd
[    2.142611] usb usb1: SerialNumber: ci_hdrc.0
[    2.147750] hub 1-0:1.0: USB hub found
[    2.151577] hub 1-0:1.0: 1 port detected
[    2.156563] imx_usb 2184200.usb: No over current polarity defined
[    2.166823] ci_hdrc ci_hdrc.1: EHCI Host Controller
[    2.171762] ci_hdrc ci_hdrc.1: new USB bus registered, assigned bus number 2
[    2.199254] ci_hdrc ci_hdrc.1: USB 2.0 started, EHCI 1.00
[    2.204926] usb usb2: New USB device found, idVendor=1d6b, idProduct=0002, bcdDevice= 6.06
[    2.213235] usb usb2: New USB device strings: Mfr=3, Product=2, SerialNumber=1
[    2.220489] usb usb2: Product: EHCI Host Controller
[    2.225376] usb usb2: Manufacturer: Linux 6.6.52-g5a0a5e71d2bd-dirty ehci_hcd
[    2.232535] usb usb2: SerialNumber: ci_hdrc.1
[    2.237597] hub 2-0:1.0: USB hub found
[    2.241419] hub 2-0:1.0: 1 port detected
[    2.251492] snvs_rtc 20cc000.snvs:snvs-rtc-lp: registered as rtc0
[    2.257628] snvs_rtc 20cc000.snvs:snvs-rtc-lp: setting system clock to 1970-01-01T00:00:00 UTC (0)
[    2.260795] ata1: SATA link down (SStatus 0 SControl 300)
[    2.266835] i2c_dev: i2c /dev entries driver
[    2.272086] ahci-imx 2200000.sata: no device found, disabling link.
[    2.282606] ahci-imx 2200000.sata: pass ahci_imx..hotplug=1 to enable hotplug
[    2.285770] Bluetooth: HCI UART driver ver 2.3
[    2.294294] Bluetooth: HCI UART protocol H4 registered
[    2.299592] Bluetooth: HCI UART protocol BCSP registered
[    2.305007] Bluetooth: HCI UART protocol LL registered
[    2.310222] Bluetooth: HCI UART protocol Three-wire (H5) registered
[    2.316527] Bluetooth: HCI UART protocol Marvell registered
[    2.322204] usbcore: registered new interface driver btusb
[    2.328901] sdhci: Secure Digital Host Controller Interface driver
[    2.335125] sdhci: Copyright(c) Pierre Ossman
[    2.339502] sdhci-pltfm: SDHCI platform and OF driver helper
[    2.347737] sdhci-esdhc-imx 2194000.mmc: Got CD GPIO
[    2.352866] sdhci-esdhc-imx 2194000.mmc: Got WP GPIO
[    2.353746] sdhci-esdhc-imx 2198000.mmc: Got CD GPIO
[    2.362916] sdhci-esdhc-imx 2198000.mmc: Got WP GPIO
[    2.363755] usbcore: registered new interface driver usbhid
[    2.373525] usbhid: USB HID core driver
[    2.384277] Galcore version 6.4.11.p2.745085
[    2.408839] mmc1: SDHCI controller on 2194000.mmc [2194000.mmc] using ADMA
[    2.408918] mmc2: SDHCI controller on 2198000.mmc [2198000.mmc] using ADMA
[    2.449354] usb 1-1: new high-speed USB device number 2 using ci_hdrc
[    2.669949] usb 1-1: New USB device found, idVendor=0424, idProduct=2514, bcdDevice= b.b3
[    2.678168] usb 1-1: New USB device strings: Mfr=0, Product=0, SerialNumber=0
[    2.700727] hub 1-1:1.0: USB hub found
[    2.704708] hub 1-1:1.0: 4 ports detected
[    2.997764] [drm] Initialized vivante 1.0.0 20170808 for 130000.gpu on minor 0
[    3.007063] mxc_vpu 2040000.vpu_fsl: VPU initialized
[    3.015259] sgtl5000 0-000a: sgtl5000 revision 0x11
[    3.024398] sgtl5000 0-000a: Using internal LDO instead of VDDD: check ER1 erratum
[    3.064731] fsl-ssi-dai 2028000.ssi: No cache defaults, reading back from HW
[    3.096416] imx-sgtl5000 sound: ASoC: driver name too long 'imx6-rex-sgtl5000' -> 'imx6-rex-sgtl50'
[    3.114109] NET: Registered PF_LLC protocol family
[    3.119542] NET: Registered PF_INET6 protocol family
[    3.125881] Segment Routing with IPv6
[    3.129662] In-situ OAM (IOAM) with IPv6
[    3.133683] sit: IPv6, IPv4 and MPLS over IPv4 tunneling driver
[    3.140396] NET: Registered PF_PACKET protocol family
[    3.145467] can: controller area network core
[    3.149926] NET: Registered PF_CAN protocol family
[    3.154731] can: raw protocol
[    3.157712] can: broadcast manager protocol
[    3.161929] can: netlink gateway - max_hops=1
[    3.166510] Bluetooth: RFCOMM TTY layer initialized
[    3.171442] Bluetooth: RFCOMM socket layer initialized
[    3.176611] Bluetooth: RFCOMM ver 1.11
[    3.180408] Bluetooth: BNEP (Ethernet Emulation) ver 1.3
[    3.185730] Bluetooth: BNEP filters: protocol multicast
[    3.190985] Bluetooth: BNEP socket layer initialized
[    3.195958] Bluetooth: HIDP (Human Interface Emulation) ver 1.2
[    3.201910] Bluetooth: HIDP socket layer initialized
[    3.207156] lib80211: common routines for IEEE802.11 drivers
[    3.212940] Key type dns_resolver registered
[    3.219552] Registering SWP/SWPB emulation handler
[    3.241846] Loading compiled-in X.509 certificates
[    3.274136] imx-ipuv3 2400000.ipu: 
[    3.278617] imx-ipuv3 2400000.ipu: revision is IPUv3H
[    3.283868] imx-ipuv3 2400000.ipu: IPU CM Regs = (ptrval)
[    3.289293] imx-ipuv3 2400000.ipu: IPU IC Regs = (ptrval)
[    3.294696] imx-ipuv3 2400000.ipu: IPU IDMAC Regs = (ptrval)
[    3.300379] imx-ipuv3 2400000.ipu: IPU DP Regs = (ptrval)
[    3.305782] imx-ipuv3 2400000.ipu: IPU DC Regs = (ptrval)
[    3.311223] imx-ipuv3 2400000.ipu: IPU DMFC Regs = (ptrval)
[    3.316802] imx-ipuv3 2400000.ipu: IPU DI0 Regs = (ptrval)
[    3.322306] imx-ipuv3 2400000.ipu: IPU DI1 Regs = (ptrval)
[    3.327798] imx-ipuv3 2400000.ipu: IPU SMFC Regs = (ptrval)
[    3.333409] imx-ipuv3 2400000.ipu: IPU CSI0 Regs = (ptrval)
[    3.338986] imx-ipuv3 2400000.ipu: IPU CSI1 Regs = (ptrval)
[    3.344577] imx-ipuv3 2400000.ipu: IPU CPMem = (ptrval)
[    3.349817] imx-ipuv3 2400000.ipu: IPU TPMem = (ptrval)
[    3.355047] imx-ipuv3 2400000.ipu: IPU DC Template Mem = (ptrval)
[    3.361182] imx-ipuv3 2400000.ipu: IPU VDI Regs = (ptrval)
[    3.389549] imx-ipuv3 2400000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    3.397071] imx-ipuv3 2400000.ipu: ipu_clk = 264000000
[    3.407087] imx-ipuv3 2800000.ipu: 
[    3.411838] imx-ipuv3 2800000.ipu: revision is IPUv3H
[    3.417553] imx-ipuv3 2800000.ipu: IPU CM Regs = (ptrval)
[    3.423104] imx-ipuv3 2800000.ipu: IPU IC Regs = (ptrval)
[    3.428510] imx-ipuv3 2800000.ipu: IPU IDMAC Regs = (ptrval)
[    3.434220] imx-ipuv3 2800000.ipu: IPU DP Regs = (ptrval)
[    3.439658] imx-ipuv3 2800000.ipu: IPU DC Regs = (ptrval)
[    3.445062] imx-ipuv3 2800000.ipu: IPU DMFC Regs = (ptrval)
[    3.450647] imx-ipuv3 2800000.ipu: IPU DI0 Regs = (ptrval)
[    3.456135] imx-ipuv3 2800000.ipu: IPU DI1 Regs = (ptrval)
[    3.461656] imx-ipuv3 2800000.ipu: IPU SMFC Regs = (ptrval)
[    3.467233] imx-ipuv3 2800000.ipu: IPU CSI0 Regs = (ptrval)
[    3.472823] imx-ipuv3 2800000.ipu: IPU CSI1 Regs = (ptrval)
[    3.478399] imx-ipuv3 2800000.ipu: IPU CPMem = (ptrval)
[    3.483656] imx-ipuv3 2800000.ipu: IPU TPMem = (ptrval)
[    3.488888] imx-ipuv3 2800000.ipu: IPU DC Template Mem = (ptrval)
[    3.494998] imx-ipuv3 2800000.ipu: IPU VDI Regs = (ptrval)
[    3.529443] imx-ipuv3 2800000.ipu: IPU DMFC NORMAL mode: 1(0~1), 5B(4,5), 5F(6,7)
[    3.537075] imx-ipuv3 2800000.ipu: ipu_clk = 264000000
[    3.544444] mxc_sdc_fb fb@0: mxcfb_probe enter
[    3.548964] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init
[    3.554693] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init - default mode 1920x1080M@60 bpp=24
[    3.563514] mxc_hdmi 20e0000.hdmi_video: Enabled HDMI clocks
[    3.569261] mxc_hdmi 20e0000.hdmi_video: Detected HDMI controller 0x13:0xa:0xa0:0xc1
[    3.577170] fbcvt: 1920x1080@60: CVT Name - 2.073M9
[    3.582303] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_disp_init exit
[    3.588318] mxc_sdc_fb fb@0: di_pixfmt:0x33424752, bpp:0x18, di:0, ipu:0
[    3.595071] mxc_sdc_fb fb@0: registered mxc display driver hdmi
[    3.601025] mxc_sdc_fb fb@0: Reconfiguring framebuffer
[    3.601038] imx-ipuv3 2400000.ipu: Channel already disabled 9
[    3.601045] imx-ipuv3 2400000.ipu: Channel already uninitialized 9
[    3.628416] mxc_sdc_fb fb@0: allocated fb @ paddr=0xF2200000, size=6220800.
[    3.630476] imx-ipuv3 2400000.ipu: init channel = 9
[    3.630490] imx-ipuv3 2400000.ipu: ipu busfreq high requst.
[    3.630516] mxc_sdc_fb fb@0: pixclock = 148500000l Hz
[    3.630522] imx-ipuv3 2400000.ipu: panel size = 1920 x 1080
[    3.630530] imx-ipuv3 2400000.ipu: pixel clk = 148500000
[    3.630561] imx-ipuv3 2400000.ipu: try ipu internal clk
[    3.630571] imx-ipuv3 2400000.ipu: rounded pix clk:176000000
[    3.630578] imx-ipuv3 2400000.ipu: try ipu ext di clk
[    3.630820] imx-ipuv3 2400000.ipu: di clk:148500000
[    3.630836] imx-ipuv3 2400000.ipu: round pixel clk:148500000
[    3.660044] imx-ipuv3 2400000.ipu: div:1
[    3.660090] mxc_sdc_fb fb@0: Y wrap disabled
[    3.660139] imx-ipuv3 2400000.ipu: IPU DMFC DP HIGH RESOLUTION: 1(0,1), 5B(2~5), 5F(6,7)
[    3.660164] imx-prg 21cc000.prg: bind prg0 ch0 with pre0
[    4.660593] imx-prg 21cc000.prg: wait for buffer ready timeout
[    4.661166] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[    4.661185] mxc_sdc_fb fb@0: Y wrap disabled
[    4.689222] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[    4.689317] mxc_sdc_fb fb@0: Update complete
[    4.689352] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE
[    4.694476] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000
[    4.830798] mxc_sdc_fb fb@0: blank = 0
[    4.830809] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_BLANK - UNBLANK
[    4.841445] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_FB_REGISTERED
[    4.847895] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_fb_registered
[    4.853832] mxc_hdmi 20e0000.hdmi_video: Hotplug interrupt received
[    4.860356] mxc_sdc_fb fb@0: Reconfiguring framebuffer
[    4.860366] mxc_sdc_fb fb@0: Reconfiguring framebuffer on the fly
[    4.860373] mxc_sdc_fb fb@0: Y wrap disabled
[    4.879261] mxc_hdmi 20e0000.hdmi_video: phy_int_stat=0x3d, phy_int_pol=0x2
[    4.879271] mxc_hdmi 20e0000.hdmi_video: EVENT=plugin
[    4.879277] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected
[    4.879284] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_read_edid
[    4.915611] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_edid_rebuild_modelist
[    5.929391] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[    6.969344] mxc_sdc_fb fb@0: MXCFB_WAIT_FOR_VSYNC: timeout 0
[    7.479334] mxc_sdc_fb fb@0: timeout when waiting for on the fly config irq
[    7.479353] fbcon_init: detected unhandled fb_set_par error, error code -110
[    7.479618] mxc_sdc_fb fb@0: Y wrap disabled
[    7.609225] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[    7.609440] mxc_sdc_fb fb@0: Update complete
[    7.641447] Console: switching to colour frame buffer device 240x67
[    7.641466] mxc_sdc_fb fb@0: Y wrap disabled
[    8.149339] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[    8.295398] mxc_hdmi 20e0000.hdmi_video: Added mode 0:
[    8.295406] mxc_hdmi 20e0000.hdmi_video: xres = 1920, yres = 1080, freq = 60, vmode = 0, flag = 17
[    8.295418] mxc_hdmi 20e0000.hdmi_video: Added mode 2:
[    8.295423] mxc_hdmi 20e0000.hdmi_video: xres = 640, yres = 480, freq = 60, vmode = 0, flag = 4
[    8.295439] mxc_hdmi 20e0000.hdmi_video: Added mode 10:
[    8.295444] mxc_hdmi 20e0000.hdmi_video: xres = 1920, yres = 1080, freq = 60, vmode = 32, flag = 2
[    8.295453] mxc_hdmi 20e0000.hdmi_video: Added mode 11:
[    8.295458] mxc_hdmi 20e0000.hdmi_video: xres = 1920, yres = 1080, freq = 50, vmode = 32, flag = 2
[    8.295466] mxc_hdmi 20e0000.hdmi_video: Added mode 12:
[    8.295471] mxc_hdmi 20e0000.hdmi_video: xres = 1920, yres = 1080, freq = 30, vmode = 32, flag = 2
[    8.295480] mxc_hdmi 20e0000.hdmi_video: Added mode 13:
[    8.295485] mxc_hdmi 20e0000.hdmi_video: xres = 1920, yres = 1080, freq = 24, vmode = 32, flag = 2
[    8.295494] mxc_hdmi 20e0000.hdmi_video: Added mode 14:
[    8.295501] mxc_hdmi 20e0000.hdmi_video: xres = 1280, yres = 720, freq = 50, vmode = 32, flag = 2
[    8.295510] mxc_hdmi 20e0000.hdmi_video: Added mode 15:
[    8.295517] mxc_hdmi 20e0000.hdmi_video: xres = 1280, yres = 720, freq = 100, vmode = 32, flag = 2
[    8.295527] mxc_hdmi 20e0000.hdmi_video: Added mode 16:
[    8.295533] mxc_hdmi 20e0000.hdmi_video: xres = 1280, yres = 720, freq = 120, vmode = 32, flag = 2
[    8.295541] mxc_hdmi 20e0000.hdmi_video: Added mode 17:
[    8.295546] mxc_hdmi 20e0000.hdmi_video: xres = 720, yres = 480, freq = 59, vmode = 32, flag = 1
[    8.295554] mxc_hdmi 20e0000.hdmi_video: Added mode 18:
[    8.295559] mxc_hdmi 20e0000.hdmi_video: xres = 720, yres = 576, freq = 50, vmode = 32, flag = 1
[    8.295602] mxc_sdc_fb fb@0: Y wrap disabled
[    8.799328] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[    9.049074] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode
[    9.049098] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode: New video mode
[    9.049113] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_set_mode_to_vga_dvi
[    9.049130] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb
[    9.049146] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_disable
[    9.049334] mxc_sdc_fb fb@0: Reconfiguring framebuffer
[    9.049367] imx-ipuv3 2400000.ipu: Channel already disabled 10
[    9.049390] imx-ipuv3 2400000.ipu: Channel already uninitialized 10
[    9.054569] mxc_sdc_fb fb@0: allocated fb @ paddr=0xF2800000, size=691200.
[    9.109150] mxc_sdc_fb fb@0: Reconfiguring framebuffer
[    9.159265] imx-ipuv3 2400000.ipu: DC stop timeout - 5 * 10ms
[    9.159309] imx-ipuv3 2400000.ipu: ipu busfreq high release.
[    9.159326] imx-ipuv3 2400000.ipu: init channel = 9
[    9.159336] imx-ipuv3 2400000.ipu: ipu busfreq high requst.
[    9.159360] mxc_sdc_fb fb@0: pixclock = 25175000l Hz
[    9.159361] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000
[    9.159367] imx-ipuv3 2400000.ipu: panel size = 640 x 480
[    9.159374] imx-ipuv3 2400000.ipu: pixel clk = 25175000
[    9.159399] imx-ipuv3 2400000.ipu: try ipu internal clk
[    9.159415] imx-ipuv3 2400000.ipu: rounded pix clk:25142857
[    9.159423] imx-ipuv3 2400000.ipu: round pixel clk:25142857
[    9.189255] imx-ipuv3 2400000.ipu: div:10
[    9.189291] mxc_sdc_fb fb@0: Y wrap disabled
[    9.189338] imx-prg 21cc000.prg: bind prg0 ch0 with pre0
[   10.189709] imx-prg 21cc000.prg: wait for buffer ready timeout
[   10.189724] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[   10.189734] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   10.202772] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   10.215809] mxc_sdc_fb fb@0: Y wrap disabled
[   10.291800] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[   10.291805] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   10.291855] mxc_sdc_fb fb@0: Update complete
[   10.291865] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE
[   10.291870] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup
[   10.291876] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed
[   10.291885] mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=0
[   10.291893] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer
[   10.291900] mxc_hdmi 20e0000.hdmi_video: final pixclk = 24780000
[   10.291908] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit
[   10.291914] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[   10.291923] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   10.304961] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   10.317995] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path
[   10.318001] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode
[   10.318011] mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk
[   10.318016] mxc_hdmi 20e0000.hdmi_video: set up AVI frame
[   10.349256] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit
[   10.349256] 
[   10.349300] mxc_sdc_fb fb@0: Y wrap disabled
[   10.429013] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   10.859330] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   10.872029] mxc_sdc_fb fb@0: Y wrap disabled
[   10.909652] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   11.379329] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   11.379381] mxc_sdc_fb fb@0: Y wrap disabled
[   11.392469] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   11.889315] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   11.952865] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   11.957594] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb exit
[   12.032604] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   12.035783] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb
[   12.112343] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   12.118257] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_disable
[   12.194275] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   12.196211] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_disable - exit
[   12.318475] mxc_sdc_fb fb@0: Reconfiguring framebuffer
[   12.318718] mxc_sdc_fb fb@1: mxcfb_probe enter
[   12.318730] mxc_sdc_fb fb@1: get of property mode_str fail
[   12.318748] mxc_sdc_fb fb@1: NO mxc display driver found!
[   12.322765] pps pps0: new PPS source ptp0
[   12.329537] fec 2188000.ethernet eth0: registered PHC device 0
[   12.331284] imx_thermal 20c8000.anatop:tempmon: Extended Commercial CPU temperature grade - max:105C critical:100C passive:95C
[   12.331383] Hot alarm is canceled. GPU3D clock will return to 64/64
[   12.332023] mxc_sdc_fb fb@1: mxcfb_probe enter
[   12.332036] mxc_sdc_fb fb@1: get of property mode_str fail
[   12.332058] mxc_sdc_fb fb@1: NO mxc display driver found!
[   12.332549] mxc_sdc_fb fb@1: mxcfb_probe enter
[   12.332561] mxc_sdc_fb fb@1: get of property mode_str fail
[   12.332576] mxc_sdc_fb fb@1: NO mxc display driver found!
[   12.339081] Micrel KSZ9021 Gigabit PHY 2188000.ethernet-1:03: attached PHY driver (mii_bus:phy_addr=2188000.ethernet-1:03, irq=POLL)
[   12.369314] imx-ipuv3 2400000.ipu: DC stop timeout - 5 * 10ms
[   12.369392] imx-ipuv3 2400000.ipu: ipu busfreq high release.
[   12.369433] imx-ipuv3 2400000.ipu: init channel = 9
[   12.369458] imx-ipuv3 2400000.ipu: ipu busfreq high requst.
[   12.369502] mxc_sdc_fb fb@0: pixclock = 148500000l Hz
[   12.369501] imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000
[   12.369522] imx-ipuv3 2400000.ipu: panel size = 1920 x 1080
[   12.369540] imx-ipuv3 2400000.ipu: pixel clk = 148500000
[   12.369610] imx-ipuv3 2400000.ipu: try ipu internal clk
[   12.369633] imx-ipuv3 2400000.ipu: rounded pix clk:176000000
[   12.369651] imx-ipuv3 2400000.ipu: try ipu ext di clk
[   12.369676] imx-ipuv3 2400000.ipu: di clk:148500000
[   12.369712] imx-ipuv3 2400000.ipu: round pixel clk:148500000
[   12.399357] imx-ipuv3 2400000.ipu: div:1
[   12.399419] mxc_sdc_fb fb@0: Y wrap disabled
[   12.399493] imx-ipuv3 2400000.ipu: DMFC high resolution has set, will not change
[   12.399529] imx-prg 21cc000.prg: bind prg0 ch0 with pre0
[   13.400273] imx-prg 21cc000.prg: wait for buffer ready timeout
[   13.401180] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[   13.401207] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   13.413351] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   13.425391] mxc_sdc_fb fb@0: Y wrap disabled
[   13.445292] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   13.467917] imx-pre 21c8000.pre: timeout waiting for PRE to run out of problematic window for shadow update
[   13.467921] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   13.467962] mxc_sdc_fb fb@0: Update complete
[   13.467973] mxc_hdmi 20e0000.hdmi_video: event=FB_EVENT_MODE_CHANGE
[   13.467981] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup
[   13.467986] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup - video mode changed
[   13.467995] mxc_hdmi 20e0000.hdmi_video: CEA mode used vic=16
[   13.468003] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer
[   13.468013] mxc_hdmi 20e0000.hdmi_video: final pixclk = 148500000
[   13.468021] mxc_hdmi 20e0000.hdmi_video: hdmi_av_composer exit
[   13.468027] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_phy_init
[   13.468037] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   13.480072] mxc_hdmi 20e0000.hdmi_video: hdmi_phy_configure
[   13.492109] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_enable_video_path
[   13.492117] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup CEA mode
[   13.492127] mxc_hdmi 20e0000.hdmi_video: hdmi_enable_audio_clk
[   13.492134] mxc_hdmi 20e0000.hdmi_video: set up AVI frame
[   13.515132] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   13.529241] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_setup exit
[   13.529241] 
[   13.529515] mxc_sdc_fb fb@0: Y wrap disabled
[   13.559250] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
				..........................
[   14.011217] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   14.039316] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   14.041223] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   14.081533] mxc_sdc_fb fb@0: Y wrap disabled
[   14.101229] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
				..........................
[   14.584323] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   14.589302] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   14.589361] mxc_sdc_fb fb@0: Y wrap disabled
[   14.614327] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
				..........................
[   15.094580] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.099295] mxc_sdc_fb fb@0: timeout when waiting for flip irq
[   15.159937] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_notify_fb exit
[   15.184587] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.186572] mxc_hdmi 20e0000.hdmi_video: mxc_hdmi_cable_connected exit
[   15.215590] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.449726] fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
[   15.451501] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.479325] Sending DHCP requests .
[   15.482506] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.898440] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.919244] ,
[   15.928448] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.958451] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.979302]  OK
[   15.981125] IP-Config: Got DHCP answer from 192.168.1.1, my address is 192.168.1.12
[   15.988457] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   15.988797] IP-Config: Complete:
[   15.998406]      device=eth0, hwaddr=00:0d:15:01:b0:f4, ipaddr=192.168.1.12, mask=255.255.255.0, gw=192.168.1.1
[   16.008553]      host=192.168.1.12, domain=, nis-domain=(none)
[   16.014420]      bootserver=0.0.0.0, rootserver=192.168.1.41, rootpath=
[   16.014428]      nameserver0=208.67.220.220
[   16.018459] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.021077] , nameserver1=208.67.222.222
[   16.035658] cfg80211: Loading compiled-in X.509 certificates for regulatory database
[   16.045982] Loaded X.509 cert 'sforshee: 00b28ddf47aef9cea7'
[   16.049470] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.053202] Loaded X.509 cert 'wens: 61c038651aabdcf94bd0ac7ff06c7248db18c600'
[   16.065353] platform regulatory.0: Direct firmware load for regulatory.db failed with error -2
[   16.074001] clk: Disabling unused clocks
[   16.078149] ALSA device list:
[   16.079480] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.081155] platform regulatory.0: Falling back to sysfs fallback for: regulatory.db
[   16.087502]   #0: imx6-rex-sgtl5000
[   16.109488] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.115993] VFS: Mounted root (nfs filesystem) on device 0:16.
[   16.122173] devtmpfs: mounted
[   16.126823] Freeing unused kernel image (initmem) memory: 1024K
[   16.133864] Run /sbin/init as init process
[   16.139491] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.169508] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.200505] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received

INIT: version 3.04 booting[   16.230512] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
/bin/hostname: invalid option -- [   16.621278] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   16.651279] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
INIT: [   16.682294] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
Entering runlevel: 3[   16.712292] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
Starting udev

[   17.295615] udevd[184]: starting version 3.2.14
[   22.689252] random: crng init done
[   22.743558] udevd[186]: starting eudev-3.2.14
[   22.889792] mxc_sdc_fb fb@1: mxcfb_probe enter
[   22.900906] mxc_sdc_fb fb@1: get of property mode_str fail
[   22.906486] mxc_sdc_fb fb@1: NO mxc display driver found!
[   22.917520] platform fb@1: deferred probe pending
[   22.938942] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.040064] caam-snvs 20cc000.caam-snvs: ipid matched - 0x3e
[   23.045825] caam-snvs 20cc000.caam-snvs: violation handlers armed - non-secure state
[   23.054427] mxc_sdc_fb fb@1: mxcfb_probe enter
[   23.058922] mxc_sdc_fb fb@1: get of property mode_str fail
[   23.059962] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.069185] mxc_sdc_fb fb@1: NO mxc display driver found!
[   23.069883] caam 2100000.crypto: Entropy delay = 3200
[   23.088553] caam 2100000.crypto: Instantiated RNG4 SH0
[   23.089973] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.097590] caam 2100000.crypto: Instantiated RNG4 SH1
[   23.105821] caam 2100000.crypto: device ID = 0x0a16010000000000 (Era 4)
[   23.113508] caam 2100000.crypto: job rings = 2, qi = 0
[   23.119982] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.121844] mxc_sdc_fb fb@1: mxcfb_probe enter
[   23.136293] mxc_sdc_fb fb@1: get of property mode_str fail
[   23.144839] mxc_sdc_fb fb@1: NO mxc display driver found!
[   23.150990] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.340505] caam algorithms registered in /proc/crypto
[   23.346002] caam 2100000.crypto: rng crypto API alg registered prng-caam
[   23.352778] caam 2100000.crypto: registering rng-caam
[   23.359552] Device caam-keygen registered
[   23.361193] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.364105] mxc_sdc_fb fb@1: mxcfb_probe enter
[   23.374530] mxc_sdc_fb fb@1: get of property mode_str fail
[   23.380068] mxc_sdc_fb fb@1: NO mxc display driver found!
[   23.387137] mxc_sdc_fb fb@1: mxcfb_probe enter
[   23.391198] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
[   23.391689] mxc_sdc_fb fb@1: get of property mode_str fail
[   23.403470] mxc_sdc_fb fb@1: NO mxc display driver found!
[   23.421202] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
sysctl: cannot stat /proc/sys/net/ipv4/tcp_syncookies: No such file or directory

[   23.662273] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
hwclock: settimeofday: Invalid argument

[   23.692282] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
Fri Mar  9 12:34:56 UTC 2018

[   24.445649] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
Setting kernel log level to 3

[   24.475672] mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received
Configuring network interfaces... ip: RTNETLINK answers: File exists
ifup skipped for nfsroot interface eth0
run-parts: /etc/network/if-pre-up.d/nfsroot: exit status 1
ip: SIOCGIFFLAGS: No such device
Starting system message bus: dbus.
Starting OpenBSD Secure Shell server: sshd
done.
Starting syslogd/klogd: done
Poky (Yocto Project Reference Distro) 5.0.9 imx6-rexultra /dev/console
imx6-rexultra login: 

There were hundereds of repeation of "mxc_hdmi 20e0000.hdmi_video: Overflow interrupt received" which I have cleaned

Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6

the link you shared includes different imx6 boards, I don't know which one you used, for standard HDMI or IPU settings in the dts files, I suggest that you can refer to the nxp official bsp

https://github.com/nxp-imx/linux-imx/tree/lf-6.6.y/arch/arm/boot/dts/nxp/imx

you can find different imx6 board settings, you can refer to that and porting this on your own board by yourself, you also can refer to the porting guide for detailed information

https://www.nxp.com/docs/en/user-guide/UG10165.pdf



Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6We have already contacted them, and they confirmed that this is the extent of the support they can provide. Development for the i.MX6 board has been discontinued. At this point, the available options are either to migrate to an i.MX8-based platform or to take ownership of the porting and maintenance effort ourselves.

The issue appears to be internal to the SoC, specifically related to the interconnection and configuration of the PRE, PRG, IPU, and HDMI blocks. This strongly suggests a device tree configuration problem rather than an external hardware fault as the HDMI driver is up and runinning.
Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6

this is third party company board, I suggest that you can contact them to get further support, because board settings are based on the HW design, they should offer the basic booting up support, if the issue is related to the imx6 SOC, we can offer the support

Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6Modified imx6qdl-rex.dtsi to add following

mxcfb1: fb@0 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "hdmi";
interface_pix_fmt = "RGB24";
mode_str ="1920x1080M@60";
default_bpp = <24>;
int_clk = <0>;
late_init = <0>;
status = "disabled";
};

mxcfb2: fb@1 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB666";
default_bpp = <16>;
int_clk = <0>;
late_init = <0>;
status = "disabled";
};

mxcfb3: fb@2 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "lcd";
interface_pix_fmt = "RGB565";
mode_str ="CLAA-WVGA";
default_bpp = <16>;
int_clk = <0>;
late_init = <0>;
status = "disabled";
};

mxcfb4: fb@3 {
compatible = "fsl,mxc_sdc_fb";
disp_dev = "ldb";
interface_pix_fmt = "RGB666";
default_bpp = <16>;
int_clk = <0>;
late_init = <0>;
status = "disabled";
};

Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6

So, If i build linux-fslc with imx_v6_v7_defconfig it uses ETNAVIV and IMX_IPUV3 drivers and enables following and I do get HDMI output

CONFIG_DRM_ETNAVIV
CONFIG_DRM_IMX
CONFIG_IMX_IPUV3_CORE
CONFIG_DRM
CONFIG_DRM_DW_HDMI

Where as linux-imx with imx_v7_defconfig uses VIVANTE and MXC_IPU. This is where I lose my HDMI output. It enables following

CONFIG_MXC_GPU_VIV
CONFIG_MXC_IPU
CONFIG_MXC_IPU_V3_PRE
CONFIG_FB_MXC_HDMI

My understanding is hdmi with working with DRM_IMX_IPUV3 and not working with MXC_IPU

Now I want to ask is it possible to use VIVANTE GPU driver with DRM_IMX_IPUV3 instead of MXC_IPU. 
I did try it but I ended up in a kernel panic which you can check here https://pastebin.com/S4VRQU9u .



Re: Problem in setting up PRE -> PRG -> IPU -> HDMI pipeline on i.MX6

linux-fslc is community bsp, not developed by the NXP, and supported by the [email protected],  linux-imx  is nxp official bsp, it seems your bsp is based on the linux-fslc, for the linux-imx, if you are interested with nxp official bsp, you can refer to the 6.3.2 Image Processing Unit (IPU) of enclosed file

Tags (1)
No ratings
Version history
Last update:
‎01-22-2026 02:22 AM
Updated by: