2291896_en-US

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

2291896_en-US

2291896_en-US

Import and start developping Using Visual Studio Code (VSC) on KW47

As the support for MCUXpresso IDE as GUI and toolchain will be stopped and will be replaced by MCUXpresso for Visual Studio Code, I am sharing here some essential steps to start development on Visual Studio Code and MCUXpresso plugin.

Preparation:

- MCUXpresso for VS Code is installed as an extension inside Microsoft VS Code - see https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...
- The rest of the toolchain including ARMGCC, west and other tools which work with MCUX for VS Code installation is available via MCUXpresso SDK option of the MCUXpresso Installer: https://www.nxp.com/design/design-center/software/development-software/mcuxpresso-software-and-tools...
- See also generic Getting Started Guide for MCUX SDK with MCUX for VS Code at: https://mcuxpresso.nxp.com/mcuxsdk/latest/html/gsd/run_a_demo_using_mcuxvsc.html


Here I will provide the procedure to import the loc_reader example from the repository.


Import the repository:

The recommended approach is to import REMOTE ARCHIVE which has a similar environment as the legacy MCUXpresso IDE. Here I will provide the procedure to import the loc_reader example from the repository

  1. From the MCUXpresso plugin, select "Import Repository", then in the "REMOTE ARCHIVE" tab, select the board, the SDK version and the location:import.pngimport.png
  2. Wait for the repository to be imported, this procedure can take several minutes.
  3. Once the import is succeed, it will appear here:imported.pngimported.png

Import demo projects and run:

  1. Once the repository is successfully imported, you can then import demo examples from the repo by selecting "Import Example from Repository":project import.pngproject import.pngthen select the demo example from "Template".
    • "AppType" should be "Freestanding application" if you want a standalone project.
    • "Location" is where the project will be located. 
    • "Toolchain" should be the Arm GNU one that you installed in preparation steps
  2. Build and run the imported project:build and run.pngbuild and run.png

Tags (1)
No ratings
Version history
Last update:
‎01-12-2026 10:33 AM
Updated by: