I want to use the STM32F429IGT6 main control chip to control the SE050 for encryption functions, but I don't know how to use or port the official middleware software package, making it impossible to implement this function.
Hi @zym ,
I would like to recommend starting from the nano package instead of the full version of MW, please kindly refer to https://github.com/NXPPlugNTrust/nano-package#porting for details.
Hope that helps,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------